Upon launching Wireshark, the user will be presented with the Wireshark capture screen. This interface allows the user to manage captured packets, and it includes the Sniffer for Bluetooth LE toolbar. In addition, it displays the hardware interfaces that are connected to the Bluetooth Low Energy Sniffer.
Note:
Always launch Wireshark in Administrator mode.
If the Sniffer for Bluetooth LE toolbar is not visible, select View>Interface Toolbars>Sniffer for Bluetooth LE.
Figure 4-2. Wireshark Capture Window
The following options are available from the capture screen in Wireshark