This feature allows the user to filter the packets that are being received based on the receiver’s RSSI. The RSSI filter shows only the packets that meet the filter criteria.
To set this filter, the user needs to use the keyword “rssi” in the capture filter on the capture screen. For example, setting the filter as “rssi >= -70” only captures the packets with an RSSI that is equal to or greater than -40 dBm. Figure 4-3. RSSI Filter Setting