Commands List
Some commands include indexes or passwords and parameters. Indexes or passwords are sent enclosed with “[]”and are coded in decimal, if numbers. Parameters are enclosed with “()” and the codification depends on the command. The default password is “PIC” but can be changed modifying the application source code. Examples:
- Example 1: DCW [10] (100000) writes 0x100000 in the control register with index equal to 10
- Example 2: IDW [PIC] (12345Q) sets the Meter Identifier to 12345Q
If the command is not properly received, decoded or processed by the application, the console will return an error message, like “Unsupported Command”, “Password Error”, ...
These are the supported commands:
| CMD | Funtion | Example | Type | Frame |
|---|---|---|---|---|
| DCR | Read DSP_CONTROL registers | Read DSP_CONTROL P_K_t register | Frame sent | DCR [09] |
| Answer |
09 P_K_T 500000 |
|||
| Note | This command can be sent without index. In this case, all the control registers values will be displayed | |||
| DCW | Write DSP_CONTROL register | Write DSP_CONTROL P_K_t register sent | Frame sent | DCW [09] (A00000) |
| Answer | set is Ok | |||
| DCM | Write DSP_CONTROL, several registers | Write DSP_CONTROL registers 38 to 41 | Frame sent | DCM(38:7B6310; 39:0; 40:51B7E89; 41:4A9D4CA) |
| Answer | Set is Ok | |||
| DSR | Read DSP_ST register | Read DSP_ST STATE_FLAG register | Frame sent | DSR [02] |
| Answer |
02 STATE_FLAG 7180020 |
|||
| Note | This command can be sent without index. In this case, all the status registers values will be displayed | |||
| DAR | Read DSP_ACC register | Read DSP_ACC I_A register | Frame sent | DAR [00] |
| Answer |
00 I_A 3000054CB |
|||
| Note | This command can be sent without index. In this case, all the accumulator registers values will be displayed | |||
| HAR | Read harmonic register | Read third harmonic register | Frame sent | HAR [03] |
| Answer |
03 I_B_R 0 |
|||
| Note | This command can be sent without index. In this case, all the accumulator registers values will be displayed | |||
| HRR | Read harmonic Irms/Vrms | Read third harmonic Irms/Vrms | Frame sent | HRR [03] |
| Answer | The calculated harmonic Irms/Vrms: Irms_Har_A(A) Irms_Har_B(A) Irms_Har(A) 0.057A 0.029A 0.028A Vrms_Har_A(V) Vrms_Har_B(V) Vrms_Har(V) 2.552V 1.262V 1.298V |
|||
| IDR | Read meter id | Frame sent | IDR | |
| Answer |
Meter ID is: 12345Q |
|||
| IDW | Write meter id (id length limited to 6 characters) | Frame sent | IDW[PIC](PI3456) | |
| Answer | Set Meter ID is Ok ! | |||
| RST | System reset | Frame sent | RST[PIC] | |
| Answer | Reset Command is Ok ! | |||
| RLD | Reload Core 1 metrology library | Frame sent | RLD[PIC] | |
| Answer | Reloaded core-1 image! Metrology lib reloaded! | |||
| DCB | Go to low power mode | Frame sent | DCB | |
| RTCW | Write meter RTC | Write RTC 20-10-19 01 09:59:00 | Frame sent | RTCW[PIC](20-10-19 01 09:59:00) |
| Answer | Set RTC is OK | |||
| RTCR | Read meter RTC | Frame sent | RTCR | |
| Answer |
Present RTC (yy-mm-dd w hh:mm:ss): 20-07-07 2 12:44:54 |
|||
| TOUW | Write meter TOU | Write TOU=8:30 T2 10:30 T3 18:30 T1 22:00 T4 | Frame sent | TOUW [PIC] (08:30 02 10:30 03 18:30 01 22:00 04) |
| Answer | Set TOU is OK | |||
| TOUR | Read meter TOU | Frame sent | TOUR | |
| Answer |
TOU table is: TOU1=08:30 T2 TOU2=10:30 T3 TOU3=18:30 T1 TOU4=22:00 T4 |
|||
| ENR | Read energy | Read current month energy | Frame sent | ENR [0] |
| Answer |
Last 0 Month Energy is: TT=4.10kWh T1=1.09kWh T2=1.65kWh T3=0.01kWh T4=1.35kWh |
|||
| ENC | Clear all energy | Frame sent | ENC [PIC] | |
| Answer | Clear energy is OK! | |||
| EVER | Read single event record | Read last 2 times Ub sag event | Frame sent | EVER[Ua][2] |
| Answer |
Last 2 times Ub Sag is: Total Num=0003 start time is 10-08 12:25 End time is 10-08 16:23 |
|||
| EVEC | Clear all event record | Frame sent | EVEC [PIC] | |
| Answer | Clear All Event is ok | |||
| MDR | Read maxim demand | Read previous 1 month maxim demand and happen time | Frame sent | MDR [1] |
| Answer |
Last 1 Month MaxDemand is: TT=26.325kW 8-4 18:45 T1=26.325kW 8-2 18:45 T2=12.350kW 8-9 14:30 T3= 8.627kW 8-6 11:15 T4= 9.483kW 8-18 23:15 |
|||
| MDC | Clear all maxim demand and happen time | Frame sent | MDC [PIC] | |
| Answer | Clear MaxDemand is ok | |||
| PAR | Read measure parameter | Read voltage | Frame sent | PAR [U] |
| Answer |
Present voltage is: Ua=221.317V Ub=223.213V Uc=219.248V |
|||
| Read current | Frame sent | PAR [I] | ||
| Answer |
Present current is: Ia=4.0114A Ib=5.0125A Ic=4.5844A Ini=0.8289A Inm=0.9491A Inmi=0.1202A |
|||
| Read active power | Frame sent | PAR [P] | ||
| Answer |
Present active power is: Pt= 750.1W Pa= 250.2W Pb= 250.8W Pc= 249.1W |
|||
| Read reactive power | Frame sent | PAR [Q] | ||
| Answer |
Present reactive power is: Qt= 360.6Var Qa=120.2Var Qb=120.3 Var Qc=120.1Var |
|||
| Read apparent power | Frame sent | PAR [S] | ||
| Answer |
Present apparent power is: St=900.8VA Sa=300.1VA Sb=300.5VA Sc=300.2VA |
|||
| Read frequency | Frame sent | PAR [F] | ||
| Answer |
Present frequency is: Freq=50.01Hz |
|||
| Read angle | Frame sent | PAR [A] | ||
| Answer |
Voltage and current angle is : Angle_A= 4.704 Angle_B= 160.699 Angle_C= 0.000 |
|||
| DCD | Load default metrology control register values | Frame sent | DCD | |
| Answer | Load Default Is Ok ! | |||
| DCS | Save metrology constants to non-volatile memory | Frame sent | DCS | |
| Answer | Save Data Is Ok ! | |||
| CAL | Automatic calibration | Single phase example | Frame sent | CAL A (Ua=220.01,Ia=4.999,Aa=59.99) |
| Answer |
It is calibrating... Calibrating Done! |
|||
| Poly phase example | Frame sent | CAL T (Ua=220.01,Ia=4.999,Aa=59.99, Ub=220.01,Ib=4.999,Ab=59.99,Uc=220.01, Ic=4.999, Ac=59.99) | ||
| Answer |
It is calibrating... Calibrating Done! |
|||
| CNF | Automatic configuration | Current Transformer example | Frame sent | CNF(MC=800,ST=0,F=50.00, G=1,Tr=1000,Rl=3.24,Ku=1651) |
| Answer | Configure Meter is ok! | |||
| Shunt resistor example | Frame sent | CNF(MC=800,ST=1,F=50.00, G=8,Tr=1000,Rl=150,Ku=1651) | ||
| Answer | Configure Meter is ok! | |||
| Rogowski Coil example | Frame sent | CNF(MC=800,ST=2,F=50.00,G=4, Tr=416.667,Rl=3.24,Ku=1651) | ||
| Answer | Configure Meter is ok! | |||
| BUF | Read waveform capture data (if a parameter is used, only a 512 samples sector is returned) | Frame sent | BUF | |
| Answer |
Waveform Capture Data... FF89BEE4 A928D0C4 … |
|||