1.1.4.4.22 DRV_RF215_SET_CHANNEL_CALLBACK Typedef
C
typedef void ( *DRV_RF215_SET_CHANNEL_CALLBACK ) (
DRV_RF215_TX_RESULT result,
uintptr_t context
);Summary
Pointer to a RF215 set channel notification callback function.
Description
This data type defines the required function signature for the RF215 driver set channel event handling callback function. A client uses DRV_RF215_SetChannelCallbackRegister to register a pointer to a function which must match the signature (parameter and return value types) specified by this data type.
Parameters
| Param | Description |
|---|---|
| result | Result of setting frequency channel through DRV_RF215_SetChannelRequest. |
| context | Value identifying the context of the application that registered the callback function. |
Returns
None.
Example
static void APP_SetChannelCb(DRV_RF215_TX_RESULT result, uintptr_t ctxt)
{
// The context handle was set to an application specific object
// It is now retrievable easily in the event handler
MY_APP_OBJ myAppObj = (MY_APP_OBJ *) ctxt;
// Set channel handling here.
}
DRV_HANDLE drvRf215Handle; // Returned from DRV_RF215_Open
MY_APP_OBJ myAppObj; // Application specific data object
DRV_RF215_SetChannelCallbackRegister(drvRf215Handle, APP_SetChannelCb,
(uintptr_t) myAppObj);Remarks
The context parameter contains a handle to the client context, provided at the time the callback function was registered using DRV_RF215_SetChannelCallbackRegister. This context value is passed back to the client as parameter. It can be any value necessary to identify the client context or instance (such as a pointer to the client's data) of the client that registered the callback.
This data type is only available if "Frequency hopping support" is enabled via MCC.