1.1.4.4.47 DRV_RF215_PLIB_SPI_SET_CALLBACK Typedef
C
typedef void ( *DRV_RF215_PLIB_SPI_SET_CALLBACK ) (FLEXCOM_SPI_CALLBACK callback, uintptr_t context);
Summary
Pointer to a PLIB function to set SPI callback.
Description
This data type defines the required function signature for the RF215 driver to register SPI callback. The registered function is called back when SPI transfer finishes.
Parameters
| Param | Description |
|---|---|
| callback | Pointer to callback function. |
| context | Value identifying the context of the client that registered the callback function. |
Returns
None.
Remarks
This data type is only available if the device does not have DMA.