1.2.12.4.3 SRV_QUEUE_Append_With_Priority Function
C
void SRV_QUEUE_Append_With_Priority(
SRV_QUEUE *queue,
uint32_t priority,
SRV_QUEUE_ELEMENT *element
);Summary
Appends an element into a priority queue.
Description
This function appends an element into a priority queue.
Precondition
The queue must have been initialized previously with function SRV_QUEUE_Init.
Parameters
| Param | Description |
|---|---|
| queue | Pointer to the queue where to append the element |
| priority | Priority of the element to be appended |
| element | Pointer to the element to be appended |
Returns
None.
Example
#define NUM_MAX_NODES 750 typedef struct node_info { SRV_QUEUE_ELEMENT queueElement; uint8_t macAddress[8] } NODE_INFO; static SRV_QUEUE nodeQueue; static NODE_INFO nodeInfo; SRV_QUEUE_Init(&nodeQueue, NUM_MAX_NODES, SRV_QUEUE_TYPE_PRIORITY); memset(nodeInfo.macAddress, 0xFF, 8); SRV_QUEUE_Append_With_Priority(&nodeQueue, 3, &nodeInfo.queueElement);
Remarks
None.