1.2.12.2 Using the Library
The SE Queue library is called to initialize a queue, add and remove elements from it and reading elements.
The following example illustrates how the SE Queue service is used by the TCP/IP - G3 ADP/MAC interface.
Example of SE Queue library usage
#include "stack/g3/net/macg3adp/drv_mac_g3adp.h" #include "drv_mac_g3adp_local.h" #include "system/sys_time_h2_adapter.h" #include "tcpip/tcpip_mac_object.h" #include "service/queue/srv_queue.h" #include "stack/g3/adaptation/adp.h" #include "stack/g3/mac/mac_wrapper/mac_wrapper_defs.h" #define DRV_MAC_G3ADP_PACKET_TX_QUEUE_LIMIT 5 #define DRV_MAC_G3ADP_PACKET_RX_QUEUE_LIMIT 5 typedef struct { SRV_QUEUE_ELEMENT queueElement; // queue element TCPIP_MAC_PACKET * pMacPacket; // pointer to the TCPIP MAC packet bool inUse; // Flag to indicate if the element is being used in a queue } DRV_G3ADP_MAC_QUEUE_DATA; static DRV_G3ADP_MAC_DRIVER _g3adp_mac_drv_dcpt; /****************************************************************************** * G3 ADP MAC local functions ******************************************************************************/ static DRV_G3ADP_MAC_QUEUE_DATA * _DRV_G3ADP_MAC_GetFreeQueueData(DRV_G3ADP_MAC_QUEUE_DATA *dataPool, uint16_t dataLen) { DRV_G3ADP_MAC_DRIVER * pMacDrv = &_g3adp_mac_drv_dcpt; DRV_G3ADP_MAC_QUEUE_DATA *ptrDataPool = dataPool; uint8_t index; uint8_t poolSize = DRV_MAC_G3ADP_PACKET_TX_QUEUE_LIMIT; if (dataPool == _rxDataPool) { poolSize = DRV_MAC_G3ADP_PACKET_RX_QUEUE_LIMIT; } for (index = 0; index < poolSize; index++, ptrDataPool++) { if (ptrDataPool->inUse == false) { if (dataLen) { // Dynamically allocate MAC Packet ptrDataPool->pMacPacket = pMacDrv->g3AdpMacData.pktAllocF(sizeof(TCPIP_MAC_PACKET), dataLen, TCPIP_MAC_PKT_FLAG_CAST_DISABLED); if (ptrDataPool->pMacPacket == NULL) { return NULL; } } ptrDataPool->inUse = true; return ptrDataPool; } } return NULL; } static DRV_G3ADP_MAC_QUEUE_DATA * _DRV_G3ADP_MAC_GetQueueDataFromMACPacket(DRV_G3ADP_MAC_QUEUE_DATA *dataPool, TCPIP_MAC_PACKET * pMacPacket) { DRV_G3ADP_MAC_QUEUE_DATA *ptrDataPool = dataPool; uint8_t index; uint8_t poolSize = DRV_MAC_G3ADP_PACKET_TX_QUEUE_LIMIT; if (dataPool == _rxDataPool) { poolSize = DRV_MAC_G3ADP_PACKET_RX_QUEUE_LIMIT; } for (index = 0; index < poolSize; index++, ptrDataPool++) { if ((ptrDataPool->inUse == true) && (ptrDataPool->pMacPacket == pMacPacket)) { return ptrDataPool; } } return NULL; } static bool _DRV_G3ADP_MAC_PutFreeQueueData(DRV_G3ADP_MAC_QUEUE_DATA *dataPool, DRV_G3ADP_MAC_QUEUE_DATA *queuedData, bool pktFreeF) { DRV_G3ADP_MAC_DRIVER * pMacDrv = &_g3adp_mac_drv_dcpt; DRV_G3ADP_MAC_QUEUE_DATA *ptrDataPool = dataPool; uint8_t index; uint8_t poolSize = DRV_MAC_G3ADP_PACKET_TX_QUEUE_LIMIT; if (dataPool == _rxDataPool) { poolSize = DRV_MAC_G3ADP_PACKET_RX_QUEUE_LIMIT; } for (index = 0; index < poolSize; index++, ptrDataPool++) { if (ptrDataPool == queuedData) { if (pktFreeF && (pMacDrv->g3AdpMacData.pktFreeF)) { // Free memory pMacDrv->g3AdpMacData.pktFreeF(ptrDataPool->pMacPacket); } ptrDataPool->inUse = false; return true; } } return false; } static void _DRV_G3ADP_MAC_RxMacFreePacket(TCPIP_MAC_PACKET * pMacPacket, const void * param) { DRV_G3ADP_MAC_DRIVER * pMacDrv = (DRV_G3ADP_MAC_DRIVER *) param; if (pMacPacket && pMacPacket->pDSeg && (pMacPacket->pDSeg->segFlags & TCPIP_MAC_SEG_FLAG_ACK_REQUIRED)) { DRV_G3ADP_MAC_QUEUE_DATA * rxQueueData =_DRV_G3ADP_MAC_GetQueueDataFromMACPacket(_rxDataPool, pMacPacket); if (rxQueueData != NULL) { _DRV_G3ADP_MAC_PutFreeQueueData(_rxDataPool, rxQueueData, true); // Update RX statistics pMacDrv->g3AdpMacData.rxStat.nRxPendBuffers--; } } } /****************************************************************************** * G3 ADP MAC local callbacks ******************************************************************************/ void _DRV_G3ADP_MAC_AdpDataCfmCallback(ADP_DATA_CFM_PARAMS* pDataCfm) { DRV_G3ADP_MAC_DRIVER * pMacDrv = &_g3adp_mac_drv_dcpt; DRV_G3ADP_MAC_QUEUE_DATA * txQueueData; if (pMacDrv->g3AdpMacData._macFlags._open) { TCPIP_MAC_PACKET * pMacPacket = (TCPIP_MAC_PACKET *)pDataCfm->nsduHandle; TCPIP_MAC_EVENT *event = &pMacDrv->g3AdpMacData.pendingEvents; ADP_RESULT result = (ADP_RESULT)pDataCfm->status; switch (result) { case G3_SUCCESS: pMacPacket->ackRes = TCPIP_MAC_PKT_ACK_TX_OK; pMacDrv->g3AdpMacData.txStat.nTxOkPackets++; *event |= TCPIP_MAC_EV_TX_DONE; break; case G3_INVALID_REQUEST: pMacPacket->ackRes = TCPIP_MAC_PKT_ACK_NET_DOWN; pMacDrv->g3AdpMacData.txStat.nTxErrorPackets++; *event |= TCPIP_MAC_EV_TX_BUSERR; break; case G3_INVALID_IPV6_FRAME: pMacPacket->ackRes = TCPIP_MAC_PKT_ACK_IP_REJECT_ERR; pMacDrv->g3AdpMacData.txStat.nTxErrorPackets++; *event |= TCPIP_MAC_EV_TX_BUSERR; break; case G3_ROUTE_ERROR: pMacPacket->ackRes = TCPIP_MAC_PKT_ACK_LINK_DOWN; pMacDrv->g3AdpMacData.txStat.nTxErrorPackets++; *event |= TCPIP_MAC_EV_TX_BUSERR; break; case G3_NO_BUFFERS: pMacPacket->ackRes = TCPIP_MAC_PKT_ACK_BUFFER_ERR; pMacDrv->g3AdpMacData.txStat.nTxErrorPackets++; *event |= TCPIP_MAC_EV_TX_BUSERR; break; default: pMacPacket->ackRes = TCPIP_MAC_PKT_ACK_MAC_REJECT_ERR; pMacDrv->g3AdpMacData.txStat.nTxErrorPackets++; *event |= TCPIP_MAC_EV_TX_ABORT; break; } pMacPacket->pktFlags &= ~TCPIP_MAC_PKT_FLAG_QUEUED; txQueueData = _DRV_G3ADP_MAC_GetQueueDataFromMACPacket(_txDataPool, pMacPacket); _DRV_G3ADP_MAC_PutFreeQueueData(_txDataPool, txQueueData, 0); // Update TX statistics pMacDrv->g3AdpMacData.txStat.nTxPendBuffers--; if (pMacPacket->ackFunc) { pMacPacket->ackFunc(pMacPacket, pMacPacket->ackParam); } } } void _DRV_G3ADP_MAC_AdpDataIndCallback(ADP_DATA_IND_PARAMS* pDataInd) { DRV_G3ADP_MAC_DRIVER * pMacDrv = &_g3adp_mac_drv_dcpt; if (pMacDrv->g3AdpMacData._macFlags._open) { DRV_G3ADP_MAC_QUEUE_DATA * rxQueueData; TCPIP_MAC_PACKET * pMacPacket; TCPIP_MAC_DATA_SEGMENT * pDSeg; // Get a Free Queue Element from the RX Queue Data Pool rxQueueData = (DRV_G3ADP_MAC_QUEUE_DATA *)_DRV_G3ADP_MAC_GetFreeQueueData(_rxDataPool, pDataInd->nsduLength); if (rxQueueData == NULL) { pMacDrv->g3AdpMacData.rxStat.nRxBuffNotAvailable++; return; } pMacPacket = rxQueueData->pMacPacket; pDSeg = pMacPacket->pDSeg; // Set pMacLayer and pNetLayer pMacPacket->pMacLayer = pDSeg->segLoad; pMacPacket->pNetLayer = pMacPacket->pMacLayer + sizeof(TCPIP_MAC_ETHERNET_HEADER); // Set Ethernet Header Type - TCPIP_ETHER_TYPE_IPV6 TCPIP_MAC_ETHERNET_HEADER* pMacHdr = (TCPIP_MAC_ETHERNET_HEADER*)pMacPacket->pMacLayer; pMacHdr->Type = TCPIP_Helper_htons(0x86DDu); // Copy data payload to Net Layer Payload memcpy(pMacPacket->pNetLayer, pDataInd->pNsdu, pDataInd->nsduLength); pDSeg->segLen = pDataInd->nsduLength + sizeof(TCPIP_MAC_ETHERNET_HEADER); pDSeg->segFlags |= TCPIP_MAC_SEG_FLAG_ACK_REQUIRED; // allow rxMacPacketAck entry // Add timestamp pMacPacket->tStamp = SYS_TMR_TickCountGet(); // just one single packet pMacPacket->next = NULL; // setup the packet acknowledgment for later use; pMacPacket->ackFunc = _DRV_G3ADP_MAC_RxMacFreePacket; pMacPacket->ackParam = pMacDrv; // Update Packet flags pMacPacket->pktFlags |= TCPIP_MAC_PKT_FLAG_QUEUED; pDSeg->next = NULL; // Append ADP packets to the ADP RX queue SRV_QUEUE_Append(&pMacDrv->g3AdpMacData.adpRxQueue, (SRV_QUEUE_ELEMENT *)rxQueueData); rxQueueData->inUse = true; // Update RX statistics pMacDrv->g3AdpMacData.rxStat.nRxSchedBuffers++; pMacDrv->g3AdpMacData.rxStat.nRxPendBuffers++; // Set RX triggered events: A receive packet is pending pMacDrv->g3AdpMacData.pendingEvents |= TCPIP_MAC_EV_RX_DONE; if (pMacDrv->g3AdpMacData.eventF) { pMacDrv->g3AdpMacData.eventF(TCPIP_MAC_EV_RX_DONE, pMacDrv->g3AdpMacData.eventParam); } } } /****************************************************************************** * G3 ADP MAC interface ******************************************************************************/ SYS_MODULE_OBJ DRV_G3ADP_MAC_Initialize(const SYS_MODULE_INDEX index, const SYS_MODULE_INIT * const init) { DRV_G3ADP_MAC_DRIVER * pMacDrv; const TCPIP_MAC_MODULE_CTRL* macControl = ((TCPIP_MAC_INIT*)init)->macControl; if (index != TCPIP_MODULE_MAC_PIC32CXMT) { return SYS_MODULE_OBJ_INVALID; // single instance } pMacDrv = &_g3adp_mac_drv_dcpt; if (pMacDrv->g3AdpMacData._macFlags._init != 0) { // already initialized return (SYS_MODULE_OBJ)pMacDrv; } if (pMacDrv->g3AdpMacData._macFlags._open != 0) { return SYS_MODULE_OBJ_INVALID; // client already connected } // Init G3 Adp Mac data memset(&pMacDrv->g3AdpMacData, 0x0, sizeof(pMacDrv->g3AdpMacData)); // use initialization data pMacDrv->g3AdpMacData.allocH = macControl->memH; pMacDrv->g3AdpMacData.callocF = macControl->callocF; pMacDrv->g3AdpMacData.freeF = macControl->freeF; pMacDrv->g3AdpMacData.pktAllocF = macControl->pktAllocF; pMacDrv->g3AdpMacData.pktFreeF = macControl->pktFreeF; pMacDrv->g3AdpMacData.pktAckF = macControl->pktAckF; // use events data pMacDrv->g3AdpMacData.eventF = macControl->eventF; pMacDrv->g3AdpMacData.eventParam = macControl->eventParam; pMacDrv->g3AdpMacData.controlFlags = macControl->controlFlags; // Init G3 ADP MAC Tx/Rx queues SRV_QUEUE_Init(&pMacDrv->g3AdpMacData.adpTxQueue, DRV_MAC_G3ADP_PACKET_TX_QUEUE_LIMIT, SRV_QUEUE_TYPE_PRIORITY); SRV_QUEUE_Init(&pMacDrv->g3AdpMacData.adpRxQueue, DRV_MAC_G3ADP_PACKET_RX_QUEUE_LIMIT, SRV_QUEUE_TYPE_SINGLE); memset(_txDataPool, 0, sizeof(_txDataPool)); memset(_rxDataPool, 0, sizeof(_rxDataPool)); pMacDrv->g3AdpMacData._macFlags._init = 1; pMacDrv->g3AdpMacData._macFlags._open = 0; pMacDrv->g3AdpMacData._macFlags._linkPresent = 0; pMacDrv->g3AdpMacData.sysStat = SYS_STATUS_BUSY; return (SYS_MODULE_OBJ)pMacDrv; } TCPIP_MAC_RES DRV_G3ADP_MAC_PacketTx(DRV_HANDLE hMac, TCPIP_MAC_PACKET * ptrPacket) { DRV_G3ADP_MAC_DRIVER * pMacDrv = &_g3adp_mac_drv_dcpt; if (hMac != (DRV_HANDLE)pMacDrv) { return TCPIP_MAC_RES_OP_ERR; } if (pMacDrv->g3AdpMacData._macFlags._open == 0) { return TCPIP_MAC_RES_INIT_FAIL; } // new packet for transmission while (ptrPacket) { DRV_G3ADP_MAC_QUEUE_DATA * txQueueData; // Get a Free Queue Element from the TX Queue Data Pool txQueueData = (DRV_G3ADP_MAC_QUEUE_DATA *)_DRV_G3ADP_MAC_GetFreeQueueData(_txDataPool, 0); if (txQueueData == NULL) { pMacDrv->g3AdpMacData.txStat.nTxQueueFull++; return TCPIP_MAC_RES_QUEUE_TX_FULL; } txQueueData->pMacPacket = ptrPacket; // Append ADP packets to the ADP TX queue SRV_QUEUE_Append_With_Priority(&pMacDrv->g3AdpMacData.adpTxQueue, (ptrPacket->pktPriority > 0), (SRV_QUEUE_ELEMENT *)txQueueData); ptrPacket->pktFlags |= TCPIP_MAC_PKT_FLAG_QUEUED; pMacDrv->g3AdpMacData.txStat.nTxPendBuffers++; if (pMacDrv->g3AdpMacData.eventF) { pMacDrv->g3AdpMacData.eventF(TCPIP_MAC_EV_TX_DONE, pMacDrv->g3AdpMacData.eventParam); } ptrPacket = ptrPacket->next; } return TCPIP_MAC_RES_OK; } TCPIP_MAC_PACKET* DRV_G3ADP_MAC_PacketRx (DRV_HANDLE hMac, TCPIP_MAC_RES* pRes, TCPIP_MAC_PACKET_RX_STAT* pPktStat) { DRV_G3ADP_MAC_DRIVER * pMacDrv = &_g3adp_mac_drv_dcpt; TCPIP_MAC_PACKET * pRxPkt = NULL; DRV_G3ADP_MAC_QUEUE_DATA * rxQueueData; TCPIP_MAC_RES mRes = TCPIP_MAC_RES_OK; if (hMac != (DRV_HANDLE)pMacDrv) { return 0; } rxQueueData = (DRV_G3ADP_MAC_QUEUE_DATA *)SRV_QUEUE_Read_Or_Remove(&pMacDrv->g3AdpMacData.adpRxQueue, SRV_QUEUE_MODE_REMOVE, SRV_QUEUE_POSITION_HEAD); if (rxQueueData == NULL) { return 0; } else { // Update RX statistics pMacDrv->g3AdpMacData.rxStat.nRxSchedBuffers--; pRxPkt = rxQueueData->pMacPacket; if (pRxPkt == NULL) { mRes = TCPIP_MAC_RES_INTERNAL_ERR; pMacDrv->g3AdpMacData.rxStat.nRxErrorPackets++; } } if (pRes) { *pRes = mRes; } // Update RX statistics pMacDrv->g3AdpMacData.rxStat.nRxOkPackets++; return pRxPkt; } TCPIP_MAC_RES DRV_G3ADP_MAC_Process(DRV_HANDLE hMac) { DRV_G3ADP_MAC_DRIVER * pMacDrv = &_g3adp_mac_drv_dcpt; if (hMac != (DRV_HANDLE)pMacDrv) { return TCPIP_MAC_RES_OP_ERR; } if (pMacDrv->g3AdpMacData._macFlags._open == 0) { return TCPIP_MAC_RES_OP_ERR; } // G3 ADP TX Process DRV_G3ADP_MAC_QUEUE_DATA * txQueueData = (DRV_G3ADP_MAC_QUEUE_DATA *)SRV_QUEUE_Read_Or_Remove(&pMacDrv->g3AdpMacData.adpTxQueue, SRV_QUEUE_MODE_REMOVE, SRV_QUEUE_POSITION_HEAD); while (txQueueData != NULL) { // Send packets to G3 ADP TCPIP_MAC_PACKET * ptrPacket = txQueueData->pMacPacket; if (ptrPacket->pNetLayer) { IPV6_HEADER *ipv6Pkt = (IPV6_HEADER *)ptrPacket->pNetLayer; uint16_t length = sizeof(IPV6_HEADER) + TCPIP_Helper_htons(ipv6Pkt->PayloadLength); ADP_DataRequest(length, (const uint8_t *)ipv6Pkt, (uint32_t)ptrPacket, true, (ptrPacket->pktPriority > 0)); } // Get next Queued Data txQueueData = (DRV_G3ADP_MAC_QUEUE_DATA *)SRV_QUEUE_Read_Or_Remove(&pMacDrv->g3AdpMacData.adpTxQueue, SRV_QUEUE_MODE_REMOVE, SRV_QUEUE_POSITION_HEAD); } return TCPIP_MAC_RES_OK; } TCPIP_MAC_RES DRV_G3ADP_MAC_ParametersGet(DRV_HANDLE hMac, TCPIP_MAC_PARAMETERS* pMacParams) { DRV_G3ADP_MAC_DRIVER * pMacDrv = &_g3adp_mac_drv_dcpt; if (hMac != (DRV_HANDLE)pMacDrv) { return TCPIP_MAC_RES_OP_ERR; } if (pMacDrv->g3AdpMacData.sysStat == SYS_STATUS_READY) { if (pMacParams) { ADP_MAC_GET_CFM_PARAMS getConfirm; ADP_DATA_NOTIFICATIONS adpDataNot; // Set ADP Data Notifications adpDataNot.dataConfirm = _DRV_G3ADP_MAC_AdpDataCfmCallback; adpDataNot.dataIndication = _DRV_G3ADP_MAC_AdpDataIndCallback; ADP_SetDataNotifications(&adpDataNot); // Get MAC address from ADP Extended Address ADP_MacGetRequestSync(MAC_WRP_PIB_MANUF_EXTENDED_ADDRESS, 0, &getConfirm); memcpy(&pMacParams->ifPhyAddress, &getConfirm.attributeValue[2], sizeof(pMacParams->ifPhyAddress)); pMacParams->processFlags = (TCPIP_MAC_PROCESS_FLAG_RX | TCPIP_MAC_PROCESS_FLAG_TX); pMacParams->macType = TCPIP_MAC_TYPE_G3ADP; pMacParams->linkMtu = TCPIP_MAC_LINK_MTU_G3ADP; pMacParams->checksumOffloadRx = TCPIP_MAC_CHECKSUM_NONE; pMacParams->checksumOffloadTx = TCPIP_MAC_CHECKSUM_NONE; pMacParams->macTxPrioNum = 2; pMacParams->macRxPrioNum = 1; } return TCPIP_MAC_RES_OK; } return TCPIP_MAC_RES_IS_BUSY; }