In MCC Project Graph window, expand
the Device Resource pane by clicking on its button on the left of Project Graph.Figure 2-40. Device Resource
Pane
Look for PIC32CXMTSH-DB component
under SHD category and add it using the Green Plus sign.Figure 2-41. Add PIC32CXMTSH-DB
Component
This automatically triggers the
activation of Core component. Click Yes to activate it.Figure 2-42. Core Component Auto
Activation
FreeRTOS component can also be
activated (it is offered), but in our case it is not needed, so click No when
prompted.
Time component.
Navigate to System Services
and add TIME component by clicking on the Green Plus sign.Figure 2-43. Add Time
Component
Right-click on TMR dependency
and select Available Satisfiers>TC0 (tc0).Figure 2-44. Select TC0 for
TMR
Modify Clock Source on TC0
component, as there is no need for accuracy in this project.Figure 2-45. Modify Clock
Source on TC0
On PIC32CXMTSH-DB Main Board
component, select PL460-EK v5 (G3 MAC RT) to be connected to Xplained Pro
Connector.Figure 2-46. Select PL460-EK v5 on
Xplained Pro Connector
This automatically adds, and configures the following components:
G3 MAC RT Driver
FLEXCOM1
PLC PVDD Monitor
ADC
Most of these components are
auto-configured by PIC32CXMTSH-DB component when components are auto-activated. Only
ADC has to be manually configured to set its prescaler and enable an interrupt, as
shown in the following figure.Figure 2-47. ADC Manual
Configuration
On G3 MAC RT component, right-click
on PCOUP dependency and select PLC PHY Coupling from Available Satisfiers.Figure 2-48. Add PLC PHY
Coupling
Add TRNG component from Peripherals
section. This will be used in this example for Random Number generation.Figure 2-49. Add TRNG Component
Finally, on PIC32CXMTSH-DB component,
enable the use of Scroll Buttons, Storage interface and Display LCD
interface. Figure 2-50. Enable Interfaces on
PIC32CXMTSH-DB
When enabling these interfaces, the
following components are automatically activated:
QSPI
SST26
SLCDC Display and Driver
The following figure shows the
complete Project Graph.Figure 2-51. Complete Project
Graph