1.2.11.4.3 CIPHER_Wrapper_AesCcmAuthDecrypt Function

C

int32_t CIPHER_Wrapper_AesCcmAuthDecrypt(uint8_t *data, uint32_t dataLen,
                                         uint8_t *iv, uint32_t ivLen,
                                         uint8_t *aad, uint32_t aadLen,
                                         uint8_t *tag, uint32_t tagLen)

Summary

Performs AES-CCM authenticated decryption of a buffer.

Description

This function performs AES-CCM authenticated decryption of a buffer.

Parameters

ParamDescription
dataPointer to buffer holding the input ciphered data. The output plain data is stored in the same buffer.
dataLenLength of the input/output data in bytes.
ivPointer to initialization vector (nonce).
ivLenLength of the nonce in bytes.
aadPointer to additional authentication data field.
aadLenLength of additional authentication data in bytes.
tagPointer to buffer holding the authentication tag.
tagLenLength of the authentication tag in bytes.

Returns

  • CIPHER_WRAPPER_RETURN_GOOD: Successful decryption and authentication
  • Any other value: Error in the decryption or authentication

Example

int32_t ret;
uint8_t nonce[] = { some initialization nonce };
uint8_t data[] = { some ciphered message };
uint8_t aad[] = { some additional authentication data };
uint8_t tag[] = { authentication tag received for verification };
uint8_t key[16] = { some key };

ret = CIPHER_Wrapper_AesCcmSetkey(key, sizeof(key));
ret = CIPHER_Wrapper_AesCcmAuthDecrypt(data, sizeof(data),
                                        nonce, sizeof(nonce),
                                        aad, sizeof(aad),
                                        tag, sizeof(tag));

Remarks

None.