Jump to main content
3.5 Running the Example
- Connect the modified Click board to
slot 3 of the Curiosity Nano Base for Click boards™.
- Connect the ATtiny1627 Curiosity Nano
to the Curiosity Nano Base for Click boards™.
- Connect the ATtiny1627 Curiosity Nano
to a computer using a USB cable.
- Download the application, as
explained in Section Get Code Examples from Atmel START or Section Get Code Examples from GitHub.
- Choose one of the two code projects
and program the ATtiny1627.
- Wave a hand or walk in front of the
sensor and observe the red LED flashing.