3.1.4.1 ICM_Initialize Function

C

void ICM_Initialize ( void );

Summary

Initializes given instance of ICM peripheral.

Description

This function initializes given instance of ICM peripheral of the device with the values configured in MCC GUI. Once the peripheral is initialized, peripheral can be used for conversion.

Precondition

MCC GUI should be configured with the right values.

Parameters

None.

Returns

None.

Example


ICM_Initialize();

Remarks

This function must be called before any other ICM function is called. This function should only be called once during system initialization.