3.1.4.11 ICM_GetRegionDescriptor Function
C
ICM_REGION_DESCRIPTOR * ICM_GetRegionDescriptor(ICM_REGION_ID regionId);Summary
Gets the pointer to the memory region descriptor.
Description
Gets the pointer to the memory region descriptor identifies with regionId parameter.
Precondition
None.
Parameters
| Param | Description |
|---|---|
| regionId | Identifies the memory region of ICM. |
Returns
Pointer to the descriptor data structure of the specified memory region.
Example
ICM_REGION_DESCRIPTOR *pRegionDescriptor;
ICM_SECONDARY_LIST icmSecList;
pRegionDescriptor = ICM_GetRegionDescriptor (ICM_REGION_0);
pRegionDescriptor->secondaryList = &icmSecList;
icmSecList.startAddress = (uint32_t)appMessageSHA1Sec;
icmSecList.transferSize = ICM_GetTransferSize(sizeof(appMessageSHA1Sec));
icmSecList.nextAddress = 0;
Remarks
None.