10 Appendix 6: Running the TCL Script
(Ask a Question)TCL scripts are provided in the design files folder under directory TCL_Scripts. If required, the design flow can be reproduced from Design Implementation till generation of job file.
To run the TCL, follow the steps below:
-
Launch the Libero software.
- Select Project > Execute Script....
- Click Browse and select
script.tclfrom the downloaded TCL_Scripts directory. - Click Run.
After successful execution of TCL script, Libero project is created within TCL_Scripts directory.
For more information about TCL scripts, refer to
mpf_an4663_v2024p1_df/TCL_Scripts/TCL_Script_readme.txt
Contact Technical Support for any queries encountered when running the TCL script.