2 Libero Design Flow
(Ask a Question)The Libero design flow involves running the following processes in the Libero SoC PolarFire:
- Synthesize
- Place and Route
- Verify Timing
- Generate FPGA Array Data
- Configure Design Initialization Data and Memories
- Configure Programming Options
- Generate Bitstream
- Run PROGRAM Action
- Export FlashPro Express JobImportant: To initialize the TCM in PolarFire using the system controller, a local parameter l_cfg_hard_tcm0_en, in the
miv_rv32_subsys_pkg.vfile should be changed to 1’b1 prior to synthesis. See the MIV_RV32 Handbook. This user guide can be downloaded from the Libero SoC Catalog.
The following figure shows these options in the Design Flow tab.