5 Appendix 1: Programming the Device Using FlashPro Express
(Ask a Question)This chapter describes how to program the PolarFire device with the Job
programming file using a FlashPro programmer. The default location of the Job file are
located at following location:
mpf_an4663_v2024p1_df\Programming_Job\top.jobTo program the PolarFire device using FlashPro Express, perform the following steps:
- Ensure that the jumper settings on the board are the same as listed in Table 2-1.Important: The power supply switch must be switched off while making the jumper connections.
- Connect the power supply cable to the J9 connector on the board.
- Connect the USB cable from the Host PC to the J5 (FTDI port) on the board.
- Power on the board using the SW3 slide switch.
- On the host PC, launch the FlashPro Express software.
- To create a new job project, click
New or
In the Project menu, select New Job Project from FlashPro Express Job, see the following figure.
Figure 5-1. FlashPro Express Job Project 
- Enter the following in the
New Job Project from FlashPro Express Job dialog box:
- Programming job file: Click
Browse, and navigate to the location where the
.jobfile is located and select the file. The default location is: <download_folder>mpf_an4663_v2024p1_df\Programming_Job. - FlashPro Express job project location:
Click Browse and navigate to the location where you want to
save the project.
Figure 5-2. New Job Project from FlashPro Express Job 
- Programming job file: Click
Browse, and navigate to the location where the
- Click OK. The required programming file is selected and ready to be programmed in the device.
- The following figure displays the
FlashPro Express window. Confirm that a programmer number appears in the Programmer
field. If it does not, confirm the board connections and click Refresh/Rescan
Programmers.
Figure 5-3. Programming the Device 
- Click RUN. When
the device is programmed successfully, a RUN PASSED status is displayed, see the
following figure.
Figure 5-4. FlashPro Express—RUN PASSED 
- Close FlashPro Express or in the Project tab, click Exit.