1.1.9.2 WDRV_WINC_BSSCtxIsValid
C
bool WDRV_WINC_BSSCtxIsValid
(
const WDRV_WINC_BSS_CONTEXT *const pBSSCtx,
bool ssidValid
)Description
Tests the elements of the BSS context to judge if their values are legal.
Precondition
None.
Parameters
| Parameters | Description |
|---|---|
| pBSSCtx | Pointer to a BSS context. |
| ssidValid | Flag indicating if the SSID within the context must be valid. |
Returns
- true - Context is valid.
- false - Context is not valid.
Remarks
A valid SSID is one which has a non-zero length. The check is optional as it is legal for the SSID field to be zero length.