8.2 Software Write Protection of the EEPROM Array
The AT24CSW01X/AT24CSW02X utilizes a software scheme that allows a portion or the entire EEPROM to be inhibited from being written to by modifying the contents of the Write Protection register (WPR). If desired, the WPR can be set so that it may no longer be modified, thereby making the current protection scheme permanent.
The status of the WPR can be determined by following a random read operation. Changing the state of the WPR is accomplished with a byte write operation with the requirements outlined in this section.
Accessing the WPR requires the use of 1011b (Bh) as the device type identifier
in the device address byte (see Device Address Byte Requirements for Accessing the Write Protection Register).
Following the device type identifier are the hardware address bits (A2, A1, A0) for which
the values are determined by the ordering code of the device (see Table 6-2). Finally, bit 0 is the Read/Write Select bit where
‘1’ is used for reading and ‘0’ is used for
writing.
| Memory Region | Device Type Identifier | Hardware Client Address Bits | R/W Select | |||||
|---|---|---|---|---|---|---|---|---|
| Bit 7 | Bit 6 | Bit 5 | Bit 4 | Bit 3 | Bit 2 | Bit 1 | Bit 0 | |
| Write Protection Register | 1 | 0 | 1 | 1 | A2 | A1 | A0 | R/W |
When accessing the Write Protection register, it is required that the A7 and A6 bits of the
word address be set to ‘11b’ respectively. The remaining bits of the word
address byte are ‘don’t care’ bits as shown in Word Address Byte Requirements for Accessing the Write Protection
Register.
| A 7 | A6 | A5 | A4 | A3 | A2 | A1 | A0 | |
|---|---|---|---|---|---|---|---|---|
| Write Protection Register | 1 | 1 | X | X | X | X | X | X |
Following the word address byte are the contents of the 8-bit Write Protection register. The register format is shown in Write Protection Register Format, and the WPR bit functions are included in Write Protection Register Bit Function.
| Operation | D7 | D6 | D5 | D4 | D3 | D2 | D1 | D0 |
|---|---|---|---|---|---|---|---|---|
| Read WPR | 0 | 0 | 0 | 0 | WPRE | WPB1 | WPB0 | WPRL |
| Write WPR | 0 | 1 | 0: No Lock | 0 | ||||
| 1: Set Lock |
| Bit | Name | Type | Description | ||
|---|---|---|---|---|---|
| 3 | WPRE | Write Protection Register Enable bit | R/W | 0 | No software write protection is enabled (Factory Default). |
1 | Write protection is set by the state of the WPB[1:0] bits. | ||||
| 2-1 | WPB[1:0] | Write-Protect Block bits | R/W | 00 |
Upper ¼ of EEPROM is write protected (Factory Default). |
01 | Upper ½ of EEPROM is write protected. | ||||
10 | Upper ¾ of EEPROM is write protected. | ||||
11 | Entire EEPROM is write protected. | ||||
| 0 | WPRL | Write-Protect Lock Bit | R/OTP | 0 | WPR can be written to; requires D5 =
0 during write (Factory Default). |
1 | WPR will become permanently locked (requires
D5 = 1) during write. | ||||
- Write Protection Register Enable bit
(WPRE), Bit 3
This bit is used to enable or disable the device software write protection feature. A logic ‘
0’ in this position will disable software write protection, and a logic ‘1’ will enable this function. - Write-Protect Block bits (WPB[1:0]),
Bits 2:1
These bits allow four levels of protection of the memory array provided that the WPRE bit is a logic ‘
1’. If the WPRE bit is a logic ‘0’, the state of the WPB[1:0] bits have no impact to device protection. The protected address ranges are found in Table 8-6. - Write-Protect Lock Bit (WPRL), Bit
0
This bit is used to permanently lock the current state of the WPR. A logic ‘
0’ indicates that the WPR can be modified, whereas a logic ‘1’ indicates the WPR has been locked and can no longer be modified. To safeguard against accidental locking of the WPR, the D5 bit must match the WPRL bit (D0 bit) sent to the device. If these bits do not match, the write cycle is aborted and the WPR contents are not modified.