35.12.2.2 Operation

Each I/O pin, Pxn, can be controlled by the registers in PORT. Each PORT group x has its own set of PORT registers, with a base address at byte address (PORT + 0x80 * group index) (A corresponds to group index 0, B corresponds to group index 1, and so on). Within that set of registers, the pin index is ‘n’, from 0 to 31.

Refer to the Pinout for additional information on available pin configuration and PORT groups.

Configuring Pins as Output

To use the Pxn pin as an output, write bit ‘n’ of the DIR register to '1'. This can also be done by writing the bit ‘n; in the DIRSET register to '1', this will avoid disturbing the configuration of other pins in that group. The ‘n’ bit in the OUT register must be written to the desired output value, this must be done first before writing the DIR bit to avoid glitching the output pin prior to setting the user desired OUT value, so the previous value of the OUT bit is not driven on the pin.

Similarly, writing an OUTSET bit to '1' will set the corresponding bit in the OUT register to '1'. Writing a bit in OUTCLR to '1' will set that bit in OUT to zero. Writing a bit in OUTTGL to '1' will toggle that bit in OUT.

Configuring Pins as Input

To use the Pxn pin as an input, the bit ‘n’ in the DIR register must be written to '0'. This can also be done by writing the bit ‘n’ in the DIRCLR register to '1', this will avoid disturbing the configuration of other pins in that group. The input value can be read from the bit ‘n’ in the IN register as soon as the INEN bit in the Pin Configuration register (PINCFGn.INEN) is written to '1'.

By default, the input synchronizer is clocked only when an input read is requested. This will delay the read operation by two cycles of the PORT clock. To remove the delay, the input synchronizers for each PORT group of eight pins can be configured to be always active, but this will increase power consumption. This is enabled by writing '1' to the corresponding SAMPLINGn bit field of the CTRL register, see CTRL.SAMPLING for details.

Using Alternative Peripheral Functions

To use the Pxn pin as one of the available peripheral functions, the corresponding PMUXEN bit of the PINCFGn register must be '1'. The PINCFGn register for the Pxn pin is at byte offset (PINCFG0 + n).

The peripheral function can be selected by setting the PMUXO or PMUXE in the PMUXm register. The PMUXO or PMUXE is at byte offset PMUX0 + (n/2). The chosen peripheral must also be configured and enabled.