1.10 RCOUNT Register
The 32-bit RCOUNT register contains the loop counter for the
REPEAT instruction. When a REPEAT instruction is
executed, RCOUNT is loaded with the repeat count of the instruction, either “lit20” for the
“REPEAT #lit20” instruction, “lit5” for the
“REPEAT #lit5” instruction or Wn register for the “REPEAT
Wn” instruction. The REPEAT loop will be executed RCOUNT + 1
time.
Note: If a
REPEAT loop is executing and gets interrupted, RCOUNT may be
cleared by the Interrupt Service Routine (ISR) to break out of the REPEAT
loop when the foreground code is re-entered.