1.13 CPU STATUS Register
Note:
- This bit may be read or cleared (not set). Clearing this bit will clear SA and SB irrespective of the value simultaneously written to SA and/or SB.
- IPL[2:0] become read only bits if
NSTDIS(INTCON1[15])=
1(nesting disabled). .
Legend: C = Clearable bit
| Name: | SR |
| Bit | 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | |
| Access | |||||||||
| Reset |
| Bit | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | |
| VF | CTX[2:0] | ||||||||
| Access | R | R | R | R | |||||
| Reset | 0 | 0 | 0 | 0 | |||||
| Bit | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | |
| OA | OB | SA | SB | OAB | SAB | IPL3 | |||
| Access | R/W | R/W | R/W | R/W | R | R/C | R/C | ||
| Reset | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
| Bit | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 | |
| IPL[2:0] | RA | N | OV | Z | C | ||||
| Access | R/W | R/W | R/W | R | R/W | R/W | R/W | R/W | |
| Reset | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | |
Bit 23 – VF Vector (Fetch) Fail Status
| Value | Description |
|---|---|
1 |
Indicates to the bus error handler that the source of the bus error is a vector fetch. The vector data read will be substituted with the contents of the Vector Fail Address (VFA) SFR. |
0 |
Indicates to the bus error handler that the source of the bus error is not a vector fetch. |
Bits 18:16 – CTX[2:0] Current (W register) Context Identifier
| Value | Description |
|---|---|
111 |
Context 7 is currently in use |
110 |
Context 6 is currently in use |
101 |
Context 5 is currently in use |
100 |
Context 4 is currently in use |
011 |
Context 3 is currently in use |
010 |
Context 2 is currently in use |
001 |
Context 1 is currently in use |
000 |
Context 0 is currently in use |
Bit 15 – OA Accumulator A Fractional Overflow Status
| Value | Description |
|---|---|
1 |
Accumulator A fractional overflow has occurred (its contents can no longer be represented as a 1.31 fractional value) |
0 |
Accumulator A not overflowed |
Bit 14 – OB Accumulator B Fractional Overflow Status
| Value | Description |
|---|---|
1 |
Accumulator A fractional overflow has occurred (its contents can no longer be represented as a 1.31 fractional value) |
0 |
Accumulator A not overflowed |
Bit 13 – SA Accumulator A Saturation/Sign Overflow ‘Sticky’ Status
| Value | Description |
|---|---|
1 |
Accumulator A is saturated or has been saturated at some time, or has overflowed into bit 71 (if saturation is disabled) |
0 |
Accumulator A is not saturated or has not overflowed into bit 71 (if saturation is disabled) |
Bit 12 – SB Accumulator B Saturation/Sign Overflow ‘Sticky’ Status
| Value | Description |
|---|---|
1 |
Accumulator B is saturated or has been saturated at some time, or has overflowed into bit 71 (if saturation is disabled) |
0 |
Accumulator B is not saturated or has not overflowed into bit 71 (if saturation is disabled) |
Bit 11 – OAB OA || OB Combined Accumulator Fractional Overflow Status
| Value | Description |
|---|---|
1 |
Accumulators A or B fractional overflow has occurred (one or both of their contents can no longer be represented as a 1.31 fractional value) |
0 |
Neither Accumulators A nor B have overflowed |
Bit 10 – SAB SA || SB Combined Accumulator ‘Sticky’ Status(1)
| Value | Description |
|---|---|
1 |
Accumulators A or B are saturated or have been saturated at some time, or have overflowed into bit 71 (if saturation is disabled) |
0 |
Neither Accumulator A nor B are saturated or have overflowed into bit 71 (if saturation is disabled) |
Bit 8 – IPL3 MSb (Most Significant bit) of CPU Priority Level Nibble
| Value | Description |
|---|---|
1 |
CPU Priority ≥ 8 (trap exception underway) |
0 |
CPU Priority < 8 (no trap exception underway) |
Bits 7:5 – IPL[2:0] CPU Interrupt Priority Level Status(2)
| Value | Description |
|---|---|
111 |
All interrupts disabled |
110 |
Level 7 interrupts enabled |
101 |
Level 6 and 7 interrupts enabled |
100 |
Level 5 through 7 interrupts enabled |
011 |
Level 4 through 7 interrupts enabled |
010 |
Level 3 through 7 interrupts enabled |
001 |
Level 2 through 7 interrupts enabled |
000 |
Level 1 through 7 interrupts enabled |
Bit 4 – RA
REPEAT Loop Active
| Value | Description |
|---|---|
1 |
REPEAT loop in
progress |
0 |
REPEAT loop not in
progress |
Bit 3 – N MCU ALU Negative
| Value | Description |
|---|---|
1 |
Result was negative |
0 |
Result was non-negative (zero or positive) |
Bit 2 – OV MCU ALU Overflow
| Value | Description |
|---|---|
1 |
Overflow occurred for signed arithmetic (in this arithmetic operation) |
0 |
No overflow occurred |
Bit 1 – Z MCU ALU ‘Sticky’ Zero
| Value | Description |
|---|---|
1 |
An operation which effects the Z bit has set it at some time in the past |
0 |
The most recent operation which effects the Z bit has cleared it (i.e., a non-zero result) |
Bit 0 – C MCU ALU Carry/Borrow
| Value | Description |
|---|---|
1 |
A carry-out from the MSb of the result occurred |
0 |
No carry-out from the MSb of the result occurred |