3.3 Compilation-Driver Interface Syntax
The compilation-driver program (xc32-gcc)
preprocesses, compiles, assembles, and links C and assembly-language modules and library
archives. This driver orchestrates the build process so that you often don't need to
know which individual programs preprocess, compile, assemble, and link. The driver calls
the appropriate individual tools to complete the requested build process.
In practice, the assembler is usually invoked via the
xc32-gcc driver, which determines from an input file's .S or .s extension that
the file contain assembly code that should be assembled. The compilation driver sends a
file with a *.S (upper case) extension through the
CPP-style preprocessor before it passes the file to the assembler while the driver sends
a file with a *.s (lower case) extension directly to
the assembler.
xc32-gcc [options] files-Wa option. The option argument
should not contain white space. See the following
example.xc32-gcc -mprocessor=32MX360F512L -I"./include" ASMfile.S
-o"ASMfile.o" -DMYMACRO=1 -Wa,-ah="ASMfile.lst"For additional information on the compilation driver, see the compiler user's guide relevant for your target device.
xc32-gcc compilation driver
from MPLAB X IDE, be sure to select the XC32 Compiler Toolchain for your project.