3.2 Assembler Interface Syntax
xc32-as [options] [sourcefiles]The order of the assembly source files determines the order in which they are assembled.
The special character sequence, -- (two hyphens not
followed by any non-space character) represents the standard input file, and can be used to
indicate that source code will be passed to the assembler via the stdin
stream.
Except for -- (as described above), any command line
argument that begins with a hyphen (-) is an option. The
options are case sensitive. It is customary to declare options before the source files;
however, this is not mandatory. Each option changes the behavior of the assembler, but no
option changes the way another option works.
test.o, either of the following options would be acceptable:-o test.o-otest.o