10.4.3 Run-Time Library Support
In order to initialize variables in data memory, the data initialization
template must be processed at start-up, before the application's main function takes
control. For C programs, this task is performed by C start-up modules in the runtime
library. Assembly language programs can also use the C start-up modules by linking with
libpic32.a for PIC32M devices or libpic32c.a for
PIC32C/SAM devices.
To utilize a start-up module, the application must allow the run-time
library to take control at device Reset. This happens automatically for C programs. The
application’s main() function is invoked after the start-up module has
completed its work. Assembly language programs should use the following naming conventions
to specify which routine takes control at device Reset.
| Main Entry Name | Description |
|---|---|
_reset | Takes control immediately after device Reset. |
main | Takes control after the start-up module completes its work. |
Note that the first entry name (_reset) includes one
leading underscore characters. The second entry name (main) includes no
leading underscore character. On device Reset, the startup module is called and it performs
the following:
- Initialize Stack Pointer.
- The data initialization template in
section
.dinitis read, causing all uninitialized sections to be cleared and all initialized sections to be initialized with values read from program memory. - Copy RAM functions from program flash to data memory an initialize bus matrix registers.
- The function main is called with no parameters.
- If main returns, the processor will reset.
The alternate start-up module is linked when the
--no-data-init linker option is specified.
It performs the same operations, except for step (2), which is omitted. The alternate start-up module is smaller than the primary module and can be selected to conserve program memory, if data initialization is not required.
Source code for both modules is provided in the device
family/lib directory of the MPLAB XC32 C compiler installation
directory. The start-up modules may be modified if necessary. For example, if an
application requires main to be called with parameters, a conditional assembly directive
may be switched to provide this support.