10.4.1 Standard Data Section Names
Traditionally, linkers based on the GNU technology support three sections in the linked binary file:
| Section Name | Description | Attribute |
|---|---|---|
.text | executable code | code |
.data | data memory that receives initial values | data |
.bss | data memory that is not initialized | bss |
The name “bss” dates back several decades, and means memory “Block Started
by Symbol”. By convention, bss memory is filled with zeros during program start-up. The
traditional section names are considered to have implied attributes as listed in the table
above. The code section attribute indicates that the section contains
executable code and should be loaded in program memory. The bss attribute
indicates that the section contains data storage that is not initialized, but will be
filled with zeros at program start-up. The data attribute indicates that
the section contains data storage that receives initial values at start-up.
Assembly applications may define additional sections with explicit attributes using the section directive described in Directives that Define Sections. For C applications, the XC32 compiler will automatically define sections to contain variables and functions as needed. For more information on the attributes of variables and functions that may result in automatic section definition, see the C compiler guide relevant for your target device.