9.5.5.4 Input Section Example
The following example is a complete linker script. It tells the linker to read all of the sections from file all.o
and place them at the start of output section outputa
which starts at location 0x10000
. All of section .input1
from file foo.o
follows immediately, in the same output section. All of section .input2
from foo.o
goes into output section outputb
, followed by section .input1
from foo1.o
. All of the remaining .input1
and .input2
sections from any files are written to output section outputc
.
SECTIONS
{
outputa 0x10000 :
{
all.o
foo.o (.input1)
}
outputb :
{
foo.o (.input2)
foo1.o (.input1)
}
outputc :
{
*(.input1)
*(.input2)
}
}