4.2.3 Pseudo Instructions
The assembler synthesizes PIC32M pseudo instructions as shown in the following table.
li
rt, imm | 32-bit load immediate |
move
rt, rs | copies rs into
rt |
la
rt, addr | a load from memory location |
jrs | jump register jr
rs |
abs
rt, rs | absolute value,
rt =
|rs| |
beq{l}
rs, label | branch equal to zero if
rs == 0 |
bge{ul}
rs, rt,
label | branch greater than equal if
rs >=
rt |
bgt{ul}
rs, rt,
label | branch greater than if
rs >
rt |
ble{ul}
rs, rt,
label | branch less than equal if
rs <=
rt |
blt{ul}
rs, rt,
label | branch less than if
rs <
rt |
bne{ul}
rs, rt,
label | branch not equal to if
rs !=
rt |
neg{u}
rt | negate rs place in rs
rs =
-rs |
rotr/ror
rt, rs,
n | rotate right, rotate
rs
n bits right, result in
rt #only pseudo insn before
mips32r2 |
rotl/rol
rt, rs,
n | rotate left, rotate
rs
n bits left, result in
rt #only pseudo insn before
mips32r2 |
sge{u}
rd, rs,
rt | set greater than equal sets
rd = 1 if
rs >=
rt |
sgt{u}
rd, rs,
rt | set greater than sets
rd = 1 if
rs >
rt |
sle{u}
rd, rs,
rt | set less than equal sets
rd = 1 if
rs <=
rt |
sne{u}
rd, rs,
rt | set not equal sets
rd = 1 if
rs !=
rt |
In the above, the bracketed letter u indicates unsigned operation and
the letter l inidcates that the likely delay slot is only executed if
the branch is taken.
Additionally, a two-operand form of all math and logic instructions is permitted, where
the first register represents both rd and rt in the full 3-operand form of the
instruction. For example add $t0, $t1 is encoded as add $t0,
$t0, $t1.
adr{cond}{.W} Rd,
label |
Register version - Load address into
|
adr{cond} Rd,
label |
PC relative version - Load Address into
|
adrl{cond} Rd,
label |
Long version - Generate two instructions to load larger addresses
into |
cpy{cond} Rd,
Rm | Alias for
mov instruction |
ldr{cond}{.W} Rt,
=expr | Loads Rt with 32-bit immediate or an address |
ldr{cond}{.W} Rt,
=label_expr | If mov
or mvn cannot be used will use literal pool to
place value and load from there |
mov32{cond} Rd,
expr | Load any 32-bit
immediate or 32-bit address into
Rd |
neg{cond} Rd,
Rm | Rd=
-Rm, alias for
RSBS{cond} Rd, Rm, #0 |
und{cond}{.W}
{#expr} | Generate an undefined
instruction for target arch - useful for forcing hard faults
expr is used to set
condition codes |
{cond} field is comprised of
instruction suffices that control conditional execution and condition flag updates. This
can be any of the following.|
|
Set the condition flags after execution |
|
|
Conditionally execute the instruction based on the
|
|
| Conditionally execute
the instruction based on the flag
condition code suffix, do not update the condition flags after execution |
|
| Specify width of the
generated instruction to be 16 or 32 bit |
Assembly directives, such as .set noat, .set nomacro, and .set
noreorder, disable these normally helpful features for cases where you
require full control over the generated code. See Symbols that Control Code
Generation.