5.7.4 If Directive
The .if expr directive marks the
beginning of a section of code that is only considered part of the source program being
assembled if the argument expr is non-zero. The end of
the conditional section of code must be marked by an .endif; optionally, you may include code for the alternative condition,
flagged by .else or .elseif.
The assembler also supports the following variants of .if.