5.7.4.9 Ifnc Directive
The .ifnc
string1,string2 directive is like .ifc, but the sense of the test is reversed: this assembles
the following section of code if the two strings are not the same.
The .ifnc
string1,string2 directive is like .ifc, but the sense of the test is reversed: this assembles
the following section of code if the two strings are not the same.
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.