10.8.1 Device-Specific Linker Script
The application source code is responsible for creating a .vector_n input section for each interrupt
vector. The C/C++ compiler creates this section when either the vector(n) or at_vector(n) attribute is
applied to the interrupt service routine. In assembly code, use the .section directive to create a new named section.
The device-specific linker script creates a single output section named
.vectors that groups all of the individual
.vector_n input sections from the project. The
start of the interrupt-vector table is mapped to the address (_ebase_address + 0x200). The default value of the _ebase_address symbol is also provided in the linker script.
For each vector, the linker script also creates a symbol named __vector_offset_n whose value is the offset
of the vector address from the _ebase_address
address.
PROVIDE(_ebase_address = 0x9D000000);
SECTIONS
{
/* Interrupt vector table with vector offsets */
.vectors _ebase_address + 0x200 :
{
/* Symbol __vector_offset_n points to .vector_n if it exists,
* otherwise points to the default handler. The
* vector_offset_init.o module then provides a .data section
* containing values used to initialize the vector-offset SFRs
* in the crt0 startup code.
*/
__vector_offset_0 = (DEFINED(__vector_dispatch_0) ? (. - _ebase_address) : __vector_offset_default);
KEEP(*(.vector_0))
__vector_offset_1 = (DEFINED(__vector_dispatch_1) ? (. - _ebase_address) : __vector_offset_default);
KEEP(*(.vector_1))
__vector_offset_2 = (DEFINED(__vector_dispatch_2) ? (. - _ebase_address) : __vector_offset_default);
KEEP(*(.vector_2))
/* … */
__vector_offset_190 = (DEFINED(__vector_dispatch_190) ? (. - _ebase_address) : __vector_offset_default);
KEEP(*(.vector_190))
}
}