5.13 __lac Intrinsic Function
The IAR __lac intrinsic function provides access to the lac
instruction, available on AVRxm devices. The lac (Load And Clear)
instruction loads the memory contents at the address held by the Z register into the Rd
register specified while simultaneously clearing those bits at that same address held by
the Z register that were set in the Rd register.
Suggested Replacement
There is no MPLAB XC8 equivalent built-in function; however, the instruction can be inserted explicitly using in-line assembly code.
Use in-line assembly to directly write an lac instruction.
Caveats
None
Examples
unsigned char loadAndClear(unsigned char regD, unsigned char * Zptr) {
unsigned char cleared = __lac(regD, Zptr);
return cleared;
}to
MPLAB XC8 code similar
to:#include <xc.h>
unsigned char lac(unsigned char v, unsigned char * addr) {
__asm__("movw r30, %[ADDR] \n\t"
"lac Z, %[Rd] \n\t"
: [Rd] "+r" (v), "+m" (*addr)
: [ADDR] "r" ((unsigned int)addr)
: "r30", "r31");
return v;
}
unsigned char loadAndClear(unsigned char regD, unsigned char * Zptr) {
unsigned char cleared = lac(regD, Zptr);
return cleared;
}Further Information
See the In-line Assembly section in the MPLAB XC8 C Compiler User's Guide for AVR MCUs for more information on adding in-line assembly.