5.15 __lat Intrinsic Function
The IAR __lat intrinsic function provides access to the
lat instruction, available on AVRxm devices. The
lat (Load And Toggle) instruction loads the memory contents at the
address held by the Z register into the Rd register specified while simultaneously
toggling those bits at that same address held by the Z register that were set in the Rd
register.
Suggested Replacement
There is no MPLAB XC8 equivalent built-in function; however, the instruction can be inserted explicitly using in-line assembly code.
Use in-line assembly to directly write an lat instruction.
Caveats
None
Examples
unsigned char loadAndToggle(unsigned char regD, unsigned char * Zptr) {
unsigned char toggled = __lat(regD, Zptr);
return toggled;
}to MPLAB XC8 code similar to:#include <xc.h>
unsigned char lat(unsigned char v, unsigned char * addr) {
__asm__("movw r30, %[ADDR] \n\t"
"lat Z, %[Rd] \n\t"
: [Rd] "+r" (v), "+m" (*addr)
: [ADDR] "r" ((unsigned int)addr)
: "r30", "r31");
return v;
}
unsigned char loadAndClear(unsigned char regD, unsigned char * Zptr) {
unsigned char toggled = lat(regD, Zptr);
return toggled;
}Further Information
See the In-line Assembly section in the MPLAB XC8 C Compiler User's Guide for AVR MCUs for more information on adding in-line assembly.