5.1 __delay_cycles Intrinsic Function
The IAR __delay_cycles intrinsic function adds code which delays execution by
the specified constant number of cycles.
Suggested Replacement
There is no equivalent built-in function, but there are library routines that perform a similar task.
Use either the _delay_ms() or _delay_us()
functions, specifying the delay time as a double argument.
Caveats
The macro F_CPU should be defined as a constant that specifies the
CPU clock frequency (in Hertz). The compiler optimizers must be enabled for accurate
delay times.
Examples
__delay_cycles(100);to
MPLAB XC8 code similar
to:#define F_CPU 1000000UL
_delay_us(100);Further Information
See the Library Functions section in the MPLAB XC8 C Compiler User's Guide for AVR MCUs for more information on these functions.