6.1 10GBASEKR Demo using Vitesse Link Partner and PolarFire Evaluation Board
(Ask a Question)Follow these steps to run the PolarFire 10GBASEKR loopback hardware demo design on the PolarFire Evaluation Board.
- Insert the copper cable to Finisar board using SFP module and connect the other end to Link Partner (LP)
- Connect the SMA cables from the PolarFire board to Finisar board as listed:
- J41 (TXP of PolarFire) -> TXP of Finisar SFP+ -> Copper cable -> Port 1 of VSC SparX-5i
- J42 (TXN of PolarFire) -> TXN of Finisar SFP+ -> Copper cable -> Port 1 of VSC SparX-5i
- J37 (RXP of PolarFire) -> RXP of Finisar SFP+ -> Copper cable -> Port 1 of VSC SparX-5i
- J38 (RXN of PolarFire) -> RXN of Finisar SFP+ -> Copper cable -> Port 1 of VSC SparX-5i
Using optical fiber cable loop back from port 1 to port 2. (In this demo, it is Port //1/2.)
- Connect the USB to serial converter cable from Link partner to host PC
- Open the associated serial terminal of LP and PolarFire board to control and monitor the status
- Program the PolarFire board with the job file
- Configure the Link Partner to support in 10GBASEKR mode. Refer to the Link Partner user manual for the commands.
- Enter the following
commands:
Terminal in Link Partner # show interface 10GigabitEthernet 1/1 status details clause-73 10GigabitEthernet 1/1: Configuration Desription: Mode: Enabled Speed/Duplex: Forced Clause 73 Media-type: SFP Flowcontrol: Off Priority-based F/C: Max. Frame: 10240 bytes Excessive Collision: Discard Frame Length Check: Disabled FEC Mode: Auto Status: Aneg: Yes (C173) Link: 10Gfdx Operational Warnings: None FEC Mode: None SFP Family: 10G DAC SFP Vendor Name: CISCO SFP Vendor P/N: SPT-SFP+C1 SFP Vendor S/N: 201110127104 SFP Vendor Revision: N SFP Date Code: 11101200 SFP Transceiver: 10GBASEKR Clause 73 Aneg Status: Completed: Yes Time since start: 24 seconds Training complete: Yes Training time: 2347 ms CM OB tap (7-bit signed): -2 (126) CP OB tap (7-bit signed): -3 (125) C0 OB tap (7-bit signed): +22 (22)
Once Auto-Negotiation and Link Training is done, the link is considered as established. The status of the link is observed in the terminal console of the Link Partner and in the UART terminal connected to PolarFire Evaluation Kit.
Terminal in PolarFire Evaluation board *** Core10GBaseKR PHY *** Starting Auto-Negotiation!! LT Link Established!! Link: Good!! Packet Testing: Total packets (msb): 0 Total packets (lsb): 42745121 Good packets (msb): 0 Good packets (lsb): 42745105 Bad packets (msb): 0 Bad packets (lsb): 0
Traffic Test
Continuous traffic is sent from the PolarFire Evaluation Kit to the Link Partner. The Link Partner then loops back the same data and sends it back to the PolarFire Evaluation Kit. The following command shows the LP data statistics.
# show interface 10GigabitEthernet 1/1 statistics: 10GigabitEthernet 1/4 Statistics:Rx Packets: 253434502Tx Packets: 253434502Rx Octets: 65892970520 Tx Octets: 65892970520 Rx Unicast: 253434502 Tx Unicast: 253434502 Rx Multicast: 0 Tx Multicast: 0 Rx Broadcast: 0 Tx Broadcast: 0 Rx Pause: 0 Tx Pause: 0 Rx 64: 0 Tx 64: 0 Rx 65-127: 0 Tx 65-127: 0 Rx 128-255: 0 Tx 128-255: 0 Rx 256-511: 253434502 Tx 256-511: 253434502 Rx 512-1023: 0 Tx 512-1023: 0 Rx 1024-1518: 0 Tx 1024-1518: 0 Rx 1519- : 0 Tx 1519- : 0 Rx Priority 0: 253434502 Tx Priority 0: 253434502 Rx Priority 1: 0 Tx Priority 1: 0 Rx Priority 2: 0 Tx Priority 2: 0 Rx Priority 3: 0 Tx Priority 3: 0 Rx Priority 4: 0 Tx Priority 4: 0 Rx Priority 5: 0 Tx Priority 5: 0 Rx Priority 6: 0 Tx Priority 6: 0 Rx Priority 7: 0 Tx Priority 7: 0 Rx Drops: 0 Tx Drops: 0 Rx CRC/Alignment: 0 Tx Late/Exc. Coll.: 0 Rx Undersize: 0 Rx Oversize: 0 Rx Fragments: 0
Orange- Represents the Received packets from PolarFire Evaluation Kit
Blue- Represents the Looped back packets from the Vitesse LP
The following command shows the PolarFire Evaluation board data statistics.
*** Core10GBaseKR PHY *** Starting Auto-Negotiation!! LT Link Established!! Link: Good!! Packet testing: Total packets (msb): 0Total packets (lsb): 253434502Good packets (msb): 0Good packets (lsb): 253434502Bad packets (msb): 0 Bad packets (lsb): 0
Orange- Represents the Transmitted packets from PolarFire Evaluation Kit
Blue- Represents the Received packets from the Vitesse LP
The following figure shows the Eye diagram with LP.

Break Link Test
The test is performed by pulling the Copper cable connected between PolarFire Evaluation board and Vitesse LP. In this case, the link will be lost. Once the cable is connected back, observe that the link is re-established.
Link: Broken!! Starting Auto-Negotiation!! LT Link Established!! Link: Good!! Packet Testing: Total packets (msb): 0 Total packets (lsb): 167147494 Good packets (msb): 0 Good packets (lsb): 122898839 Bad packets (msb): 0