1.35 TCC Timer Mode
This example shows how to use the TCC module in timer mode to generate periodic interrupt.
Description
TCC is configured in timer mode and generates periodic interrupt. LED is toggled in the interrupt handler to indicate periodic callback.
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/tcc/tcc_timer_mode/firmware.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description | 
|---|---|
| pic32ck_gc01_cult.X | MPLABX Project for PIC32CK GC01 Curiosity Ultra board | 
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Board | 
|---|---|
| pic32ck_gc01_cult.X | PIC32CK GC01 Curiosity Ultra board | 
Setting Up PIC32CK GC01 Curiosity Ultra Board
- Connect the Debug USB port on the board to the computer using a micro USB cable
 
Running the Application
- Build and Program the application using its IDE
 - Observe that the LED blinks once every second
 
| Board | LED Name | 
|---|---|
| PIC32CK GC01 Curiosity Ultra board | LED0 |