1.6 CAN FD Interrupt
This example application shows how to use the CAN module to transmit and receive CAN FD messages in interrupt mode.
Description
This application transmits CAN FD message to CAN Bus and receives CAN FD message from CAN Bus. To run this application, two evaluation boards of same type are required. These boards acts as different nodes on the CAN bus. Same application is programmed onto both the boards. Boards are connected to PC via UART. While running the application, user can send and receive CAN FD messages between the boards using UART console applications running on the PC.
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/can/can_fd_operation_interrupt_timestamp/firmware.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description | 
|---|---|
| pic32ck_gc01_cult.X | MPLABX Project for PIC32CK GC01 Curiosity Ultra board | 
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Board | 
|---|---|
| pic32ck_gc01_cult.X | PIC32CK GC01 Curiosity Ultra board | 
Setting Up PIC32CK GC01 Curiosity Ultra Board
- Connect PIC32CK-GC01 Curiosity Ultra board to another PIC32CK-GC01 Curiosity
                        Ultra board as per the pin connections shown below
PIC32CK-GC01 Curiosity Ultra board - 1 PIC32CK-GC01 Curiosity Ultra board - 2 CANH, CAN0 CANH, CAN0 CANL, CAN0 CANL, CAN0 GND, CAN0 GND, CAN0  - Connect the Debug USB port on the board to the computer using a micro USB cable
 
Running the Application
- Open the Terminal application (Ex.:Tera term) on the computer
 - Connect to the PKOB4 Virtual COM port and configure the serial settings as
                        follows:
- Baud : 115200
 - Data : 8 Bits
 - Parity : None
 - Stop : 1 Bit
 - Flow Control : None
 
 - Build and Program the application using its IDE
 - In the console associated with board 1, press “0” to transmit a CAN FD message
 - Transmitted message description and status will be displayed in the console window of board 1
 - Received message will be displayed in the console window of board 2
 - Follow the sequence below to send and receive different messages:
- Press ‘1’ on board 1
 - Press ‘2’ on board 1
 - Press ‘3’ on board 1
 - Press ‘4’ on board 1
 - Press ‘0’ on board 2
 - Press ‘1’ on board 2
 - Press ‘2’ on board 2
 - Press ‘3’ on board 2
 - Press ‘4’ on board 2
 
 - If the steps are executed in this sequence, the final output in the consoles
                    will be as below (console on the left is the transmitter (board 1) and the one
                    on the right is receiver (board 2)):