1 Harmony 3 Peripheral Library Application Examples for PIC32CK-GC/SG Family
The following applications are provided to demonstrate the typical or interesting usage models of one or more peripheral libraries.
| Name | Description | 
|---|---|
| AC Sleepwalking | This example application shows how to use the AC Peripheral library to perform a single shot comparison in standby sleep mode periodically and wake up the device when the comparator output toggles | 
| ADC Blocking | This example application shows how to use the ADC Peripheral library in blocking mode to convert analog input on a ADC channel | 
| ADC DMA Scan | This example application shows how to use the ADC Peripheral library in scan mode to convert multiple analog input on a ADC channels and transfer the ADC result using DMA | 
| ADC Interrupt | This example application shows how to use the ADC Peripheral library in in interrupt mode to convert multiple analog inputs | 
| CAN FD Blocking | This example application shows how to use the CAN module to transmit and receive CAN FD messages in polling mode | 
| CAN FD Interrupt | This example application shows how to use the CAN module to transmit and receive CAN FD messages in interrupt mode | 
| CAN Blocking | This example application shows how to use the CAN module to transmit and receive normal CAN messages in polling mode | 
| Clock Configuration | This example application shows how to configure the clock system to run the device at maximum frequency. It also outputs a prescaled clock signal on a GPIO pin for measurement and verification | 
| DMA CRC-32 Generation | This example application demonstrates how to use the DMA peripheral to compute 32-bit Cyclic Redundancy Checksum (CRC) | 
| DMAC USART Echo | This example application demonstrates USART transfer with DMA to receive 10 bytes and echo back the received bytes | 
| DMAC Memory Transfer | This example application demonstrates how to use the DMAC peripheral to do a memory to memory transfer | 
| DSU CRC32 Generate | This example application demonstrates how to use the DSU Peripheral library to compute 32-bit Cyclic Redundancy Checksum (CRC) | 
| EIC Interrupt | This example application demonstrates how to generate interrupt using the EIC on switch press and indicate it through an LED | 
| EVSYS Trigger | This example application demonstrates how to use the EVSYS Peripheral library to setup autonomous, low-latency and configurable communication between peripherals | 
| FCW Read Write | This example application demonstrates how to use the FCW to erase and program the internal Flash memory | 
| FREQM Measurement | This example application demonstrates how to use the FREQM peripheral to measure the frequency of the internal RC Oscillator | 
| MPU Cache Coherency | This example shows how to maintain cache coherency by allocating DMA buffers in non-cacheable SRAM region defined by MPU | 
| PM Wakeup Using EIC | This application demonstrates entering the low power modes and exiting it using the EIC | 
| PM Wakeup Using RTC | This example demonstrates entering the low power modes and exiting it using the RTC | 
| PORT Polling | This example application demonstrate how to poll the switch input, and indicate the switch status using the LED | 
| RSTC Reset Cause | This example shows how to use the RSTC peripheral to indicate the cause of the device reset | 
| RTC Alarm Interrupt | This example shows how to use the RTC to configure the time and generate the alarm | 
| RTC Periodic Interrupt | This example application shows how to use the RTC to generate periodic interrupts | 
| SERCOM I2C EEPROM Read Write | This example application demonstrates how to use the SERCOM peripheral to write and read from the I2C serial EEPROM memory | 
| SERCOM SPI EEPROM Read Write | This example application demonstrates how to use the SERCOM SPI peripheral to write and read from the SPI serial EEPROM memory | 
| SERCOM SPI Interrupt | This example application shows how to use SERCOM SPI PLIB with external loop back to write and then read back an array of data in interrupt mode | 
| SERCOM USART Blocking | This example application demonstrates how to use the SERCOM peripheral in USART mode to transfer block of data in a blocking manner | 
| SERCOM USART Interrupt | This example application demonstrates how to use the SERCOM peripheral in USART mode to transfer data in a non-blocking manner | 
| SERCOM USART Ring Buffer | This example application demonstrates how to use the SERCOM peripheral in USART ring buffer mode to transfer data in a non-blocking manner | 
| SQI Flash Read Write | This example application demonstrates how to use the SQI Peripheral library to perform erase, write and read operation with the on-board SST26 SQI Serial Flash memory | 
| Systick Periodic Interrupt | This example shows how to use the SysTick to generate periodic interrupts | 
| TCC PWM Generation | This example application shows how to use the TCC to generate a 2 or 3 phase PWM signals for motor control with dead time | 
| TCC Capture Mode | This example shows how to use the TCC module in capture mode to measure duty cycle and frequency of an external input | 
| TCC Compare Mode | This example shows how to use the TCC module in compare mode to generate different waveforms | 
| TCC Timer Mode | This example shows how to use the TCC module in timer mode to generate periodic interrupt | 
| TRAM Erase On Tamper Detect | This example application shows how to configure and use tamper detect feature of RTC and TrustRam | 
| TRNG Random Number | This example shows how to use the TRNG Peripheral library to generate and read a random number | 
| TrustZone Systick Periodic Timeout | This example application shows how to use the SysTick to generate periodic interrupts on both Secure and Non-secure modes | 
| TrustZone Secure TCC Demonstration | This example application performs a PWM signal applied on PD20 pin (LED0) based on TCC0 peripheral | 
| WDT Timeout | This example shows how to generate a Watchdog timer reset by emulating a deadlock |