1.9 DMA CRC-32 Generation
This example application demonstrates how to use the DMA peripheral to compute 32-bit Cyclic Redundancy Checksum (CRC).
Description
The DMA unit provides support for calculating a CRC-32 value for data passing through any DMA channel.
This example application computes the 32-bit CRC value for the polynomial (0x4C11DB7) using below data source for the CRC engine in DMA peripheral
- It uses a DMA Channel with software trigger to initiate a memory-memory transfer from the source buffer to the destination buffer. Once the transfer is completed a 32-bit CRC will be generated for the source buffer.
 
Once the hardware CRC are generated using above method, it is validated using a software-calculated CRC value.
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/dma/dma_crc32_generate/firmware.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description | 
|---|---|
| pic32ck_gc01_cult.X | MPLABX Project for PIC32CK GC01 Curiosity Ultra board | 
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Board | 
|---|---|
| pic32ck_gc01_cult.X | PIC32CK GC01 Curiosity Ultra board | 
Setting Up PIC32CK GC01 Curiosity Ultra Board
- Connect the Debug USB port on the board to the computer using a micro USB cable
 
Running the Application
- Open the Terminal application (Ex.:Tera term) on the computer
 - Connect to the PKOB4 Virtual COM port and configure the serial settings as
                        follows:
- Baud : 115200
 - Data : 8 Bits
 - Parity : None
 - Stop : 1 Bit
 - Flow Control : None
 
 - Build and Program the application using its IDE
 - LED indicates the success or failure:
- LED is turned ON when the DMA memory transfer is successful and hardware CRC values matched with the software calculated CRC value
 - Following table provides the LED name
Board LED Name PIC32CK GC01 Curiosity Ultra board LED0  
 - Observe output message in console as follows:
- Expected CRC Value for the polynomial (0x4C11DB7) is
                                (0xb70b4c26)

 
 - Expected CRC Value for the polynomial (0x4C11DB7) is
                                (0xb70b4c26)