3.9.4.2.4 Proximity Light Sensor Example Application on PIC32CM LS00 Curiosity Nano + Touch Evaluation Kit
Description
This application demonstrates how to interface VCNL4200 with Curiosity Nano Explorer board and PIC32CM LS00 Curiosity Nano + Touch evaluation kit. VCNL4200 integrates a high sensitivity proximity sensor, ambient light sensor and 940 nm IRED into one small package and it is present in Curiosity Nano Explorer Board. Proximity sensor detects nearby objects whereas ambient light sensor detects light intensity. Based on the light source and object's distance from the sensor, the value generated by ambient light sensor and proximity sensor varies.
Modules/Technology Used
- Peripheral Modules
- PM
- SYSTICK
- SERCOM2
- SERCOM3
- EVSYS
- STDIO
The following figure provides the MCC Harmony project graph with all the components.

Hardware Used
Software/Tools Used
Refer to the Project Manifest present in
harmony-manifest-success.yml under the project folder
pic32cm_ls00_cnano_proximity/firmware/src/config/pic32cm_ls00_cnano.
- Refer to the Release Notes to know the MPLAB X IDE and MCC Plug-in version
Due to Microchip regularly updates tools, occasionally issue(s) could be discovered while using the newer versions of the tools. If the project does not seem to work and version incompatibility is suspected, it is recommended to double-check and use the same versions that the project was tested with. To download original version of MPLAB Harmony v3 packages, refer to the document How to Use the MPLAB Harmony v3 Project Manifest Feature (DS90003305).
Setup
- Connect the PIC32CM LS00 Curiosity Nano
+ Touch evaluation kit to the host PC using a Type-A male to micro-B USB cable. Plug the
cable into the Micro-B USB (Debug USB) port on the evaluation kit
Programming Hex File
The pre-built hex file can be programmed by following the below steps.
- Open MPLAB X IDE
- Close all existing projects in IDE, if any project is opened
- Go to
File>Import>Hex/ELF File - In the Import Image File window,
- Create Prebuilt Project,
- Click the Browse button to select the prebuilt hex file
- Select Device as PIC32CM5164LS00048
- Ensure the proper tool is selected under Hardware Tool and click the Next button
- Select Project Name and Folder,
- Select appropriate project name and folder and click the Finish button
- Create Prebuilt Project,
- In MPLAB X IDE, click the Make and Program Device button to program the device
- Follow the steps in Running the Demo section
Programming/Debugging Application Project
- Open the project
(
pic32cm_ls00_cnano_proximity/firmware/proximity_pic32cm_ls00_cnanogroup) in MPLAB X IDE - Right click on
proximity_pic32cm_ls00_cnanogroupfile and go toOpen Required projects>Open All Projects - Then, right click on the non-secure project and click Set as Main Project
- Ensure
PIC32CM LS00 Curiosity Nanois selected as hardware tool to program/debug the application - Build the code and program the device by clicking on the Make and Program button in MPLAB X IDE tool bar
- Follow the steps in Running the Demo section
Running the Demo
- Open the Tera Term/PuTTY terminal application on the PC (from the Windows® Start menu by pressing the Start button)
- Set the baud rate to 115200
- To Reset the device, run this command
ipecmd.exe -P32CM5164LS00048 -TPNEDBG -OKfrom the following locationC:/Program Files/Microchip/MPLABX/v6.20/mplab_platform/mplab_ipe
- The console prints the value of
proximity sensor and ambient light sensor as shown in the figure below

- The value of proximity sensor increases as an object moves closer to the sensor and decreases as the object moves further away from the sensor
- The value of ambient light sensor
increases when light source is close to the sensor and decreases as the light source
moves further away from the sensor

Comments
- Reference Training Module: Arm TrustZone Getting Started Application on PIC32CM LS60 (Arm Cortex-M23) MCUs
- This application demo builds and
works out of box by following the instructions in Running the Demo section. If the
user needs to enhance/customize this application demo, should use the MPLAB Harmony v3
Software framework. Refer to the following links to setup and build the applications
using MPLAB Harmony.
- How to Setup MPLAB Harmony v3 Software Development Framework (DS90003232)
- How to Build an Application by Adding a New PLIB, Driver, or Middleware to an Existing MPLAB Harmony v3 Project (DS90003253)
- Video - How to Set up the Tools Required to Get Started with MPLAB® Harmony v3 and MCC
- Create a new MPLAB Harmony v3 project using MCC
- Update and Configure an Existing MHC-based MPLAB Harmony v3 Project to MCC-based Project