7.3.16 Function ac_win_get_config_defaults()
Initializes an ACIFC window configuration structure to default values.
void ac_win_get_config_defaults( struct ac_win_config *const cfg)
Note: This function should be called to prepare all new instances of ACIFC window configuration structures before they are further modified by the user application.
The default configuration is as follows:Window mode is disabled
Peripheral event from ACWOUT is disabled
Generate the window peripheral event when the comparison is done
Window interrupt enabled when the evaluation of the common input voltage is done
| Data direction | Parameter name | Description |
|---|---|---|
[out] | cfg |
ACIFC window configuration structure pointer |