11.1.3 Erasing Program Flash Memory
The minimum erase block varies by device as shown in the memory organization table. Only through the use of an external programmer, or through ICSP™ control, can larger blocks of program memory be bulk erased. Word erase in the Flash array is not supported.
For example, when initiating an erase sequence from a microcontroller with erase row size of 32 words, a block of 32 words (64 bytes) of program memory is erased. The TBLPTR<21:6> bits point to the block being erased. The TBLPTR<5:0> bits are ignored.
The NVMCON1 register commands the erase operation. The NVMREG bits must be set to point to the Program Flash Memory. The WREN bit must be set to enable write operations. The FREE bit is set to select an erase operation.
The NVM unlock sequence described in the 11.1.2 NVM Unlock Sequence section must be used which guards against accidental writes. This is sometimes referred to as a long write.
A long write is necessary for erasing the internal Flash. Instruction execution is halted during the long write cycle. The long write is terminated by the internal programming timer.