The following figure shows the recommended power-down sequence to place
the device in BSR mode (Backup Mode with SDRAM in Self-refresh mode to save the context). A
combination of the LPM and SHDN signals, both outputs of the Shutdown Controller (SHDWC),
requests a special powering mode to the external power supply where VDDIODDR is maintained.
These outputs are supplied by VBAT present in BSR mode. In a similar way to the power-down
sequence, the NRST signal must be asserted prior to turning the SAMA7G5 power supplies
off.
Figure 11-6. Recommended Power Sequence at BSR Mode Entry
Table 11-14. BSR Mode Entry Timing Specification
Symbol
Parameter
Conditions
Min
Max
Unit
tSHDN
SHDN delay at backup mode
entry
Delay from SHDN low to NRST
low
0
–
ms
tRSTPD
NRST delay at
power-down
Delay from NRST low to the
first supply out of its operating range
0
–
ms
The following figure shows the recommended power-up sequence to wake up
the device from BSR mode. Upon a Wake-up event (WKUP pin, RTC alarm, etc.), the Shutdown
Controller automatically toggles its SHDN output back to VBAT to request the external power
supply to restart. This power-up sequence is the same as the one shown in Figure 11-2. In particular, the supply groups definition is the same. The LPM pin is
not automatically reset, and therefore the external power supply may enter a power saving
state at wake-up. To make the power supply return to normal operation, the LPM pin must be
software-reset in the SHDWC as soon as possible in the wake-up process.Figure 11-7. Recommended Power Sequence at
Wake-Up from BSR Mode
Table 11-15. Wake-Up from BSR Mode Timing Specification(1)
Symbol
Parameter
Conditions
Min
Max
Unit
t0
VDDIN33 delay
Delay from SHDN high to
VDDIN33 turn-on
0
–
ms
t1
VDDIN33 to periphery group
delay
Delay from established
VDDIN33 to the first periphery group supply established
-0.3
–
ms
t2
Periphery group to VDDCORE
delay
Delay from the last periphery
group established supply to VDDCORE supply turn-on
0
–
ms
t3
Reset delay at
power-up
From established VDDCORE to
NRST high
8
–
ms
Note:
The term "established" refers to a power supply established at 90% of its final
value.