The following figure shows the recommended power-down sequence to place
the device in Backup mode. The SHDN signal, output of the Shutdown Controller (SHDWC),
signals the shutdown request to the external power supply. This output is supplied by VBAT
present in Backup mode. In a similar way to the power-down sequence, the NRST signal must
be asserted prior to turning the device power supplies off.Figure 11-4. Recommended Power Sequence at Backup Mode Entry
Delay from NRST low to the
first supply out of its operating range
0
–
ms
The following figure shows the recommended power-up sequence to wake up
the device from Backup mode. Upon a Wake-up event (WKUP pin, RTC alarm, etc.), the Shutdown
Controller automatically toggles its SHDN output back to VBAT to request the external power
supply to restart. This power-up sequence is the same as the one shown in Figure 11-2. In particular, the supply groups definition is the same.
Figure 11-5. Recommended Power Sequence at Wake-Up from Backup Mode
Table 11-13. Wake-Up from Backup Mode Timing Specification(1)
Symbol
Parameter
Conditions
Min
Max
Unit
t0
VDDIN33 delay
Delay from SHDN high to
VDDIN33 turn-on
0
–
ms
t1
VDDIN33 to periphery group
delay
Delay from established
VDDIN33 to the first established periphery group supply
-0.3
–
ms
t2
Periphery group to VDDCORE
delay
Delay from the last
periphery group established supply to VDDCORE supply turn-on
0
–
ms
t3
Reset delay at
power-up
From established VDDCORE to
NRST high
8
–
ms
Note:
The term "established" refers to a power supply established at 90% of its final
value.