1.1.2.6.10 DRV_AK4954_SamplingRateGet Function
uint32_t DRV_AK4954_SamplingRateGet(DRV_HANDLE handle)
Summary
This function gets the sampling rate set on the DAC AK4954.
Description
This function gets the sampling rate set on the DAC AK4954.
Preconditions
The DRV_AK4954_Initialize routine must have been called for the specified AK4954 driver instance.
DRV_AK4954_Open must have been called to obtain a valid opened device handle.
Parameters
Parameters | Description |
---|---|
handle | A valid open-instance handle, returned from the driver's open routine |
Returns
None.
Remarks
None.
Example
uint32_t baudRate; _\/\/ myAK4954Handle is the handle returned \/\/ by the DRV_AK4954_Open function._ baudRate = DRV_AK4954_SamplingRateGet(myAK4954Handle);
C
uint32_t DRV_AK4954_SamplingRateGet(DRV_HANDLE handle);