1.1.2.6.1 DRV_AK4954_MicGainGet Function
uint8_t DRV_AK4954_MicGainGet(DRV_HANDLE handle)Summary
This function gets the microphone gain for the AK4954 Codec.
Description
This functions gets the current microphone gain programmed to the Codec AK4954.
Preconditions
The DRV_AK4954_Initialize routine must have been called for the specified AK4954 driver instance.
DRV_AK4954_Open must have been called to obtain a valid opened device handle.
Parameters
| Parameters | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open routine |
Returns
Microphone gain, in range 0-31.
Remarks
None.
Example
_\/\/ myAppObj is an application specific object._ MY_APP_OBJ myAppObj; uint8_t gain; _\/\/ myAK4954Handle is the handle returned \/\/ by the DRV_AK4954_Open function._ gain = DRV_AK4954_MicGainGet(myAK4954Handle);
C
uint8_t DRV_AK4954_MicGainGet(DRV_HANDLE handle);