1.1.2.6.3 DRV_AK4954_MicMuteOff Function
void DRV_AK4954_MicMuteOff(DRV_HANDLE handle)Summary
Umutes th AK4954's microphone input.
Description
This function unmutes the AK4954's microphone input.
Preconditions
The DRV_AK4954_Initialize routine must have been called for the specified AK4954 driver instance.
DRV_AK4954_Open must have been called to obtain a valid opened device handle.
Parameters
| Parameters | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open routine |
Returns
None.
Remarks
None.
Example
_\/\/ myAppObj is an application specific object._ MY_APP_OBJ myAppObj; _\/\/ myAK4954Handle is the handle returned \/\/ by the DRV_AK4954_Open function._ DRV_AK4954_MicMuteOff(myAK4954Handle); _\/\/AK4954 microphone unmuted_
C
void DRV_AK4954_MicMuteOff(DRV_HANDLE handle);