1.1.4.6.4 DRV_WM8904_SamplingRateSet Function
void DRV_WM8904_SamplingRateSet(DRV_HANDLE handle, uint32_t samplingRate)Summary
This function sets the sampling rate of the media stream.
Description
This function sets the media sampling rate for the client handle.
Preconditions
The DRV_WM8904_Initialize routine must have been called for the specified WM8904 driver instance.
DRV_WM8904_Open must have been called to obtain a valid opened device handle.
Parameters
| Parameters | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open routine |
| samplingRate | Sampling frequency in Hz |
Returns
None.
Remarks
None.
Example
_// myWM8904Handle is the handle returned // by the DRV_WM8904_Open function._
DRV_WM8904_SamplingRateSet(myWM8904Handle, 48000); _//Sets 48000 media sampling rate_C
void DRV_WM8904_SamplingRateSet(DRV_HANDLE handle, uint32_t samplingRate);