1.1.4.6.5 DRV_WM8904_VolumeGet Function
uint8_t DRV_WM8904_VolumeGet(DRV_HANDLE handle, DRV_WM8904_CHANNEL channel)Summary
This function gets the volume for WM8904 Codec.
Description
This functions gets the current volume programmed to the Codec WM8904.
Preconditions
The DRV_WM8904_Initialize routine must have been called for the specified WM8904 driver instance.
DRV_WM8904_Open must have been called to obtain a valid opened device handle.
Parameters
| Parameters | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open routine |
| channel | argument indicating Left or Right or Both channel volume to be modified |
Returns
None.
Remarks
None.
Example
_// myAppObj is an application specific object._ MY_APP_OBJ myAppObj; uint8_t volume; _// myWM8904Handle is the handle returned // by the DRV_WM8904_Open function._ volume = DRV_WM8904_VolumeGet(myWM8904Handle, DRV_WM8904_CHANNEL_LEFT);
C
uint8_t DRV_WM8904_VolumeGet(DRV_HANDLE handle, DRV_WM8904_CHANNEL channel);