1 Harmony 3 Driver and System Service Application Examples for SAM E70/S70/V70/V71 Family

The following applications are provided to demonstrate the typical or interesting usage models of one or more peripheral libraries.
NameDescription
Console Debug System Service using UARTThis example application demonstrates the UART based console and debug system service
Console Debug System Service using USBThis example application demonstrates the USB based console and debug system service
EEPROM Emulator Library Read WriteThis application example demonstrates how to read and write to the Emulated EEPROM memory space using the EEPROM Emulator library
FAT File System using NVM and SDMMC MediaThis application shows an example of using the FAT File System to access files across multiple media (NVM, SDMMC)
FAT File System using NVM and SDSPI MediaThis application shows an example of using the FAT File System to access files across multiple media (NVM, SDSPI)
FAT Filesystem throughput using SDMMC MediaThis application calculates throughput by Writing and Reading data into a SD-Card at High Speed using the MPLAB Harmony File System and the SDMMC driver
FAT Filesystem using NVM and SST26 MediaThis application shows an example of using the FAT File System to access multiple files across multiple media (NVM, SQI FLASH)
FAT Filesystem using NVM MediaThis application shows an example of implementing a FAT disk in the device internal Flash memory
FAT Filesystem using RAM MediaThis application shows an example of using the FAT File System to access RAM media
FAT Filesystem using SDMMC MediaThis application shows an example of using the FAT File System to access and modify the contents of a SD card using the SDMMC driver
FAT Filesystem using SDSPI MediaThis application shows an example of using the FAT File System to access and modify the contents of a SD card using the SDSPI driver and the SPI PLIB
FAT Filesystem using SST26 MediaThis application shows an example of using the FAT File System to access SQI based SST26 flash media
FreeRTOS BasicThis example application demonstrates context switching between four tasks of different priorities. Two tasks run periodically while the other two tasks are event driven
FreeRTOS Task NotificationThis example application is to illustrate the FreeRTOS Task Notification feature which is used as a light weight binary semaphore
FreeRTOS Tickless BasicThis example application blinks an LED to show the FreeRTOS threads that are running and to indicate status in the FreeRTOS tickless idle mode
I2C Driver Asynchronous - I2C EEPROMThis example application shows how to use the I2C driver in asynchronous mode to perform operations on the EEPROM
I2C Driver Asynchronous - Multi ClientThis example application demonstrates the multi-client feature of the asynchronous mode of the I2C driver by communicating with an external EEPROM and a temperature sensor
I2C Driver Synchronous - I2C EEPROMThis example application shows how to use the I2C driver in synchronous mode to perform operations on the EEPROM
I2C Driver Synchronous - Multi ClientThis example application demonstrates the multi-client feature of the synchronous mode of the I2C driver by communicating with an external EEPROM and a temperature sensor
I2C EEPROM AT24 Driver - EEPROM Read WriteThis example application shows how to use the AT24 driver to perform read and write operations on AT24 series of EEPROM
Memory Driver Asynchronous - NVM SST26 Read WriteThis example application shows how to use the Memory driver in asynchronous mode to perform block operations on the NVM and the SST26 media’s
Memory Driver Synchronous - NVM SST26 Read WriteThis example application shows how to use the Memory driver in synchronous mode to perform block operations on the NVM and the SST26 media’s
MPFS Filesystem using NVM MediaThis application shows an example of implementing a MPFS disk in device Internal Flash memory
SDMMC Driver Asynchronous - SDMMC Read WriteThis example application shows how to use the SDMMC driver in asynchronous mode to perform block operations on the SD Card Media
SDSPI Driver Synchronous - SDSPI Read WriteThis example application shows how to use the SDSPI driver in synchronous mode to perform block operations on the SD Card Media
SPI Driver Asynchronous - Multi ClientThis example demonstrates how to use single instance of the SPI driver in asynchronous mode to communicate with multiple EEPROMs
SPI Driver Asynchronous - Self Loopback Multi ClientThis example demonstrates how to use the SPI driver in asynchronous mode to achieve self-loop back between multiple clients
SPI Driver Synchronous - Multi ClientThis example demonstrates how to use single instance of the SPI driver in synchronous mode to communicate with multiple EEPROMs
SPI Driver Synchronous - Self Loopback Multi ClientThis example demonstrates how to use the SPI driver in synchronous mode to achieve self-loop back between multiple clients in RTOS environment
SPI EEPROM AT25 Driver - EEPROM Read WriteThis example application shows how to use the AT25 driver to perform read and write operations on AT25 series of EEPROM
SST26 SQI Flash Driver - Flash Read Write in Quad IO ModeThis example application shows how to use the SST26 SQI flash driver to perform block operations on the On-Board SST26 Flash memory in Quad IO mode
SST26 SQI Flash Driver - Flash Read Write in SPI ModeThis example application shows how to use the SST26 driver to perform block operations on the On-Board SST26 Flash memory in SPI mode
Time System Service Multi-clientThis example application demonstrates the multi-client system timer functionality
USART Driver Asynchronous - USART EchoThis example echoes the received characters over the console using the USART driver in asynchronous mode
USART Driver Asynchronous - USART Multi InstanceThis example echoes the received characters over the two consoles using the USART driver in asynchronous mode
USART Driver Synchronous - USART EchoThis example echoes the received characters over the console using the USART driver in synchronous mode
USART Driver Synchronous - USART Multi InstanceThis example echoes the received characters over the two consoles using the USART driver in synchronous mode