1.26 SPI Driver Asynchronous - Multi Client

This example demonstrates how to use single instance of the SPI driver in asynchronous mode to communicate with multiple EEPROMs.

Description

This example write and read data to and from two separate EEPROM connected over the same SPI bus by using the multi client feature of the driver. The example also demonstrates how to setup two different EEPROM transfers at different baud rates.

Downloading and Building the Application

To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.

Path of the application within the repository is apps/driver/spi/async/spi_multi_slave/firmware.

To build the application, refer to the following table and open the project using its IDE.

Project NameDescription
sam_e70_xult.XMPLABX project for SAM E70 Xplained Ultra Evaluation Kit
sam_e70_xult_freertos.XMPLABX project for SAM E70 Xplained Ultra Evaluation Kit
sam_v71_xult.XMPLABX project for SAM V71 Xplained Ultra Evaluation Kit
sam_v71_xult_freertos.XMPLABX project for SAM V71 Xplained Ultra Evaluation Kit

Setting Up the Hardware

The following table shows the target hardware for the application projects.

Project NameDescription
sam_e70_xult.X

sam_e70_xult_freertos.X

SAM E70 Xplained Ultra Evaluation Kit
sam_v71_xult.X

sam_v71_xult_freertos.X

SAM V71 Xplained Ultra Evaluation Kit