1.16 I2C Driver Asynchronous - I2C EEPROM

This example application shows how to use the I2C driver in asynchronous mode to perform operations on the EEPROM.

Description

This example uses the I2C driver in asynchronous mode to communicate with the EEPROM to perform write and read operations in Bare-Metal environment. This application uses I2C driver to read and write data from an on-Board AT24MAC402 EEPROM device.

Downloading and Building the Application

To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.

Path of the application within the repository is apps/driver/i2c/async/i2c_eeprom/firmware.

To build the application, refer to the following table and open the project using its IDE.

Project NameDescription
sam_e70_xult.XMPLABX project for SAM E70 Xplained Ultra Evaluation Kit
sam_e70_xult_freertos.XMPLABX project for SAM E70 Xplained Ultra Evaluation Kit
sam_v71_xult.XMPLABX project for SAM V71 Xplained Ultra Evaluation Kit
sam_v71_xult_freertos.XMPLABX project for SAM V71 Xplained Ultra Evaluation Kit

Setting Up the Hardware

The following table shows the target hardware for the application projects.

Project NameDescription
sam_e70_xult.X

sam_e70_xult_freertos.X

SAM E70 Xplained Ultra Evaluation Kit
sam_v71_xult.X

sam_v71_xult_freertos.X

SAM V71 Xplained Ultra Evaluation Kit

Setting Up SAM E70 Xplained Ultra Evaluation Kit

  • Connect the Debug USB port on the board to the computer using a micro USB cable

Setting Up SAM V71 Xplained Ultra Evaluation Kit

  • Connect the Debug USB port on the board to the computer using a micro USB cable